Skip to main content
User.44
Associate II
Sep 11, 2020 2:15 AM UTC
Solved

Use v2.2-r0 TF-A to burn to stm32mp157c-ev1 via STM32_Programmer_CLI, USB is not supported

Hi

The terminal printing information is as follows.

This TF-A will start properly in EMMC.

0693W000003RMSDQA4.png

In the docs/plat/stm32mp1.rst file, I saw that USB is not supported. May I ask how to modify it so that it can be burned via USB

0693W000003RMSNQA4.png

Regards

User.44

This topic has been closed for replies.
Bernard PUEL
Bernard PUELBest answer
ST Technical Moderator
Sep 14, 2020 1:13 PM UTC

Here is the new file you can replace "Makefile.sdk" from the V2.0.0/.../tf-a-stm32mp-2.2.r1-r0/ directory (obviously, you need to remove .txt extension).

5 replies

Olivier GALLIEN
ST Technical Moderator
Sep 11, 2020 8:23 AM UTC

Hi @文�?� �?​ 

This is a known issue we have recently discovered internally also.

I come back to you shortly.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Bernard PUEL
ST Technical Moderator
Sep 14, 2020 12:17 PM UTC

In the developer package, the Makefile.sdk for tf-a was not well generated and it needs revision for the "serialboot" build.

A new Makefile.sdk will be delivered in this post that will solve this issue.

User.44
User.44Author
Associate II
Sep 14, 2020 12:32 PM UTC

Hi Bernard PUEL

The article

Bernard PUEL
Bernard PUELBest answer
ST Technical Moderator
Sep 14, 2020 1:13 PM UTC

Here is the new file you can replace "Makefile.sdk" from the V2.0.0/.../tf-a-stm32mp-2.2.r1-r0/ directory (obviously, you need to remove .txt extension).

User.44
User.44Author
Associate II
Sep 14, 2020 1:33 PM UTC

Hi Bernard PUEL

Thank you very much for bothering me for 3 days