Skip to main content
Grodriguez
Associate III
Jul 14, 2026 8:42 AM UTC
Solved

Undefined instruction exceptions due to compiler-generated NEON code in TF-A

We are experiencing issues on STM32MP13 when using TF-A with OP-TEE due to an "Undefined instruction" exception during low-power entry.

When TF-A is built with a standard arm-*-gnueabihf toolchain, the compiler is allowed to generate NEON instructions because the STM32MP1 platform enables:

ARM_WITH_NEON := yes

In our case, GCC generates NEON instructions when compiling lib/compiler-rt/builtins/udivmoddi4.c, which is reached from udelay() during the low-power sequence. At that point, however, the VFP/NEON unit is disabled, so execution aborts with an "Undefined instruction" exception.

Relevant TF-A build settings:

  • ARM_CORTEX_A7 := yes  (from STM32MP1 platform settings)
  • ARM_WITH_NEON := yes  (from STM32MP1 platform settings)
  • AARCH32_SP := optee
  • CTX_INCLUDE_FPREGS=0

Relevant compiler options:

  • -mcpu=cortex-a7  (generated by TF-A from ARM_CORTEX_A7 := yes)
  • -mfpu=neon  (generated by TF-A from ARM_WITH_NEON := yes)
  • -ffreestanding
  • -fno-builtin
  • -Os

We have verified that replacing udelay() with a simple NOP loop (for testing purposes) is enough to work around the problem.

Building TF-A with options that prevent compiler-generated NEON instructions (such as -mfloat-abi=soft) also avoids the exception.

Interestingly, the STM32MP1 platform already contains a special case for sp_min:

ifeq ($(AARCH32_SP),sp_min)
# Disable Neon support: sp_min runtime may conflict with non-secure world
TF_CFLAGS += -mfloat-abi=soft
endif

We are wondering whether a similar approach should also be considered when AARCH32_SP=optee, or whether there is another recommended way to avoid executing compiler-generated NEON instructions in this code path.

Any feedback is welcome.

Regards,

Guillermo

Grodriguez
GrodriguezBest answer
Associate III
Jul 21, 2026 8:05 AM UTC

1 reply

Grodriguez
GrodriguezAuthorBest answer
Associate III
Jul 21, 2026 8:05 AM UTC