Skip to main content
jhi
Senior
Jan 29, 2022 1:55 PM UTC
Solved

Uboot not executing board_init function?

I'm using the bootlin buildroot branch: st/2021.02.

I want to run a certain function on init of the Uboot (board_init function), like the ones used for the DK1 and DK2. My problem is that the function doesn't seem to be called. I have tried to debug the problem and put printf and put commands to get something shown on terminal, but nothing gets printed on terminal. I also tried to put while(1); function, to the board_init function, but the boot just goes on. When using make uboot-rebuild, I can see that the stm32mp1.c is compiled after I have changed it. I also deleted everything on output/images, so that the new images are really made. I also tried to do the same to board_late_init function, but no change.

What am I doing wrong? Is the function not really called? If not, why? And if yes, why isn't it even stopping with while(1) endless loop?

This topic has been closed for replies.
jhi
jhiBest answer
Senior
Feb 1, 2022 10:58 AM UTC

My stupid failure. Because of Arm trusted firmware, I have to rebuild it also to see the changes I made to u-boot.

1 reply

jhi
jhiAuthorBest answer
Senior
Feb 1, 2022 10:58 AM UTC

My stupid failure. Because of Arm trusted firmware, I have to rebuild it also to see the changes I made to u-boot.