Skip to main content
Associate III
Jul 9, 2024 8:27 AM UTC
Solved

The issue of using discrete power supply in STM32MP157D

The power supply part of the board I made myself did not use "stpmic", but used a discrete power supply. I encountered an issue when porting OpenSTLinux (5.1.0). After modifying the power supply in the "u boot" device tree and using "STM32CubeProgrammer" to download, it kept downloading repeatedly, as shown in the following figure:
1.png
I have modified these positions: under "i2c4", the "pmic: stpmic@33 All nodes have been deleted, and the following content has been added to the root node:
vddcore: regulator-vddcore {
        compatible = "regulator-fixed";
regulator-name = "vddcore";
regulator-min-microvolt = <1200000>;
regulator-max-microvolt = <1350000>;
regulator-always-on;
        regulator-boot-on;
};
 
    v3v3: regulator-3p3v {
        compatible = "regulator-fixed";
        regulator-name = "v3v3";
        regulator-min-microvolt = <3300000>;
        regulator-max-microvolt = <3300000>;
        regulator-always-on;
        regulator-boot-on;
    };
 
    v1v8_audio: regulator-v1v8-audio {
        compatible = "regulator-fixed";
        regulator-name = "v1v8_audio";
        regulator-min-microvolt = <1800000>;
        regulator-max-microvolt = <1800000>;
        regulator-always-on;
        regulator-boot-on;
    };
 
    vdd: regulator-vdd {
        compatible = "regulator-fixed";
        regulator-name = "vdd";
        regulator-min-microvolt = <3300000>;
        regulator-max-microvolt = <3300000>;
        regulator-always-on;
        regulator-boot-on;
    };
 
    vdd_usb: regulator-vdd-usb {
        compatible = "regulator-fixed";
        regulator-name = "vdd_usb";
        regulator-min-microvolt = <3300000>;
        regulator-max-microvolt = <3300000>;
        regulator-always-on;
        regulator-boot-on;
    };
This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
Jul 15, 2024 7:30 AM UTC

Hi @zengyixiang 

nice to see you solved the issue.

Could you share the solution as it could be of interest of other members of the forum who fall into similar issue?

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

6 replies

Associate III
Jul 9, 2024 8:33 AM UTC

Has anyone encountered this situation before? How should we solve it

Associate III
Jul 10, 2024 1:19 AM UTC

Is anybody there

PatrickF
ST Employee
Jul 10, 2024 10:07 AM UTC

Hi @zengyixiang 

Hard to solve your issue with few informations.

Maybe linked to DDR issue which mean uBoot crash at some point of time (use STM32DDRFW-UTIL to confirm behavior) . Maybe issue with mixed-up DDR signals (e.g. DQS or DM mixed with DQ bytes lanes) which create trouble as soon as non-32-bits data are needed from DDR.

Any HW issue which could generate a reset (e.g. supply drop, conflicts on signals, etc...) ?

Any memory size issue (i.e. UBoot or else trying to use unavailable DDR memory which could corrupt some other DDR area due to mirroring) ?

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Associate III
Jul 15, 2024 1:04 AM UTC

Thank you, I have identified the issue

PatrickF
PatrickFBest answer
ST Employee
Jul 15, 2024 7:30 AM UTC

Hi @zengyixiang 

nice to see you solved the issue.

Could you share the solution as it could be of interest of other members of the forum who fall into similar issue?

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent