Solved
"Synchronous Abort" handler, esr 0x96000006, far 0x0
- 1 reply
- 93 views
I wonder why this is happening after U-boot has booten up?
It seems that something is NULL.
D/TC:? 0 tee_ta_close_session:484 Destroy session
Error: eth1@482c0000 address not set.
D/TC:? 0 tee_ta_init_session_with_context:562 Re-open trusted service a8cfe406-d4f5-4a2e-9f8d-a25dc754c099
F/TC:? 0 pta_scmi_invoke_command:404 SCMI command 0x3 ptypes 0x3
F/TC:? 0 pta_scmi_invoke_command:404 SCMI command 0x4 ptypes 0x651
D/TC:? 0 tee_ta_close_session:465 csess 0x821301f0 id 1
D/TC:? 0 tee_ta_close_session:484 Destroy session
No ethernet found.
�7�[r�[999;999H�[6n�8No EFI system partition
No EFI system partition
Failed to persist EFI variables
D/TC:? 0 tee_ta_init_pseudo_ta_session:303 Lookup pseudo TA ab7a617c-b8e7-4d8f-8301-d09b61036b64
D/TC:? 0 tee_ta_init_pseudo_ta_session:315 Open rng.pta
D/TC:? 0 tee_ta_init_pseudo_ta_session:330 rng.pta : ab7a617c-b8e7-4d8f-8301-d09b61036b64
F/TC:? 0 plat_prng_add_jitter_entropy:74 0x1C
D/TC:? 0 tee_ta_close_session:465 csess 0x821301f0 id 1
D/TC:? 0 tee_ta_close_session:484 Destroy session
D/TC:? 0 tee_ta_init_session_with_context:562 Re-open trusted service a8cfe406-d4f5-4a2e-9f8d-a25dc754c099
F/TC:? 0 pta_scmi_invoke_command:404 SCMI command 0x3 ptypes 0x3
F/TC:? 0 pta_scmi_invoke_command:404 SCMI command 0x4 ptypes 0x651
D/TC:? 0 tee_ta_close_session:465 csess 0x82130040 id 1
D/TC:? 0 tee_ta_close_session:484 Destroy session
"Synchronous Abort" handler, esr 0x96000006, far 0x0
elr: 00000000840900b4 lr : 0000000084090b24 (reloc)
elr: 00000000fa0b40b4 lr : 00000000fa0b4b24
x0 : 0000000000000000 x1 : 00000000f8005218
x2 : 0000000000000000 x3 : 0000000000000005
x4 : 0000000000000000 x5 : 00000000fa15f14f
x6 : 0000000000000000 x7 : 0000000000000002
x8 : 00000000f8004e90 x9 : fffffffffffffff0
x10: f80051c800000000 x11: f803531000000000
x12: 2e4af5d406e4cfa8 x13: 99c054c75da28d9f
x14: 00000000f8005058 x15: 00000000f8005060
x16: 00000000fa0c3634 x17: 45afd5bf09c54952
x18: 00000000f8021d50 x19: 00000000f805a1b0
x20: 00000000f8073dd0 x21: 0000000000000000
x22: 00000000fa153c34 x23: 00000000f8075e90
x24: 00000000f8035520 x25: 0000000000000000
x26: 0000000000000000 x27: 00000000fa172c6a
x28: 0000000000000000 x29: 00000000f80050e0
Code: aa0103f0 d61f0200 128004a0 d65f03c0 (f9400002)
Resetting CPU ...
resetting ...
INFO: PSCI Power Domain Map:
INFO: Domain Node : Level 4, parent_node 4294967295, State ON (0x0)
INFO: Domain Node : Level 3, parent_node 0, State ON (0x0)Link to my DT for U-boot: https://github.com/DanielMartensson/Watermelon-Wine-1A/tree/linux-testing/watermelon-wine-os%2Flayers%2Fmeta-watermelon-wine%2Fmx%2Fwatermelon-wine-1a%2FCA35%2FDeviceTree%2Fwatermelon-wine-1a%2Fu-boot
I have attached the output log as well.