Skip to main content
UVV
Associate III
November 3, 2024
Question

stpmic1-regulator warnings

Hey there,

I have a custom stm32mp153c based board. I adapted bootloaders/optee/kernel from scarthgap branch of meta-st-stm32mp and have everything booting (tf-a 2.8, u-boot 2022.10, optee 3.19, kernel 6.1.28). The only remaining warnings I have are these:

root@stm32mp1:~# dmesg | grep pmic
[ 0.459590] stpmic1 2-0033: PMIC Chip Version: 0x21
[ 0.497690] stpmic1-regulator 5c009000.i2c:stpmic@33:regulators: Failed to create device link (0x180) with 2-0033
[ 0.506580] stpmic1-regulator 5c009000.i2c:stpmic@33:regulators: Failed to create device link (0x180) with 2-0033
[ 0.516882] stpmic1-regulator 5c009000.i2c:stpmic@33:regulators: Failed to create device link (0x180) with 2-0033

 

I found only two threads mentioning the issue, but couldn't figure out how to fix it and even got an impression that these are somehow expected?

https://community.st.com/t5/stm32-mpus-embedded-software-and/platform-5a001000-display-controller-deferred-probe-pending-why/m-p/710943

https://community.st.com/t5/stm32-mpus-products/various-issues-when-starting-kernel-on-custom-stm32mp151aac/m-p/598410

 

Any hints where the warnings come from?

 

Thanks,

Vyacheslav

This topic has been closed for replies.

3 replies

PatrickF
ST Employee
November 4, 2024

Hi @UVV 

Scarthgap is not yet supported by OpenSTLinux (will come soon).

Wait few weeks or go back to Mickeldore: https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ecosystem_release_note#OpenSTLinux_for_Arm-C2-AE_Cortex-C2-AE-A

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
UVV
UVVAuthor
Associate III
November 4, 2024

Perhaps I was not clear with my statement, but I don't use scarthgap branch, I'm still on kirkstone. I only took the bootloader/kernel from the scarthgap branch. I see that kernel version mentioned in your link is newer though. I could give it a try.

 

As a yocto maintainer, I'm not sure I like your advise to use non LTS version, and why updates are provided in mickeldore rather than in LTS branch.

PatrickF
ST Employee
November 4, 2024

Hi,

I'm not SW expert, just try to find out rationale of your warning messages.

We provide a new ecosystem major release almost every year, but as Yocto LTS is every two years, we then have one intermediate release on a 'non-LTS' Yocto version.

If you want only LTS Yocto, as you do, you should stick to our latest Kirkstone release https://wiki.st.com/stm32mpu-ecosystem-v4/wiki/STM32_MPU_ecosystem_release_note#OpenSTLinux_-28Arm-C2-AE_Cortex-C2-AE-A7-29

I guess it is important to have TF-A, OpTee and uBoot versions aligned to our ecosystem releases.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent