Skip to main content
Visitor II
Aug 19, 2026 1:18 PM UTC
Question

STM32MP257F + IMX335: std::bad_alloc when configuring 640x640 secondary libcamera stream

Hello ST Team,

I am working on an AI-based Driver Monitoring System on an STM32MP257F board using an IMX335 MIPI CSI camera, libcamera,
GStreamer and STAI-MPU.

I am facing a memory allocation / segmentation fault issue when using a custom STAI-MPU application.

------------------------------------------------------------
HARDWARE
------------------------------------------------------------

Board:
STM32MP257F

Camera:
Sony IMX335 MIPI CSI

Camera interface:
CSI / DCMIPP

Display:
Weston / Wayland

Camera source:
LIBCAMERA

------------------------------------------------------------
SOFTWARE
------------------------------------------------------------

libcamera:
0.3.0+dirty

Python:
3.12

The exact OpenSTLinux/X-LINUX-AI version and other system information can be provided if required.

------------------------------------------------------------
KNOWN-GOOD ST APPLICATION
------------------------------------------------------------

I tested the official ST face-recognition example:

https://github.com/STMicroelectronics/meta-st-x-linux-ai/tree/main/recipes-samples/face-recognition

The official application works correctly on the same STM32MP257F board and the same IMX335 camera.

The working application reports:

camera framerate: 30
camera frame width: 760
camera frame height: 568
camera source: LIBCAMERA

libcamera configures:

(0) 760x568-RGB565
(1) 128x128-BGR888

The application runs successfully.

------------------------------------------------------------
CUSTOM AI APPLICATION
------------------------------------------------------------

I replaced the AI models with my own proprietary STAI-MPU models.

The important model characteristics are:

Model 1:
Input: 640x640x3
INT8
STAI-MPU .nb format

Model 2:
Input: 192x192x3
INT8
STAI-MPU .nb format

Both models successfully load through STAI-MPU.

The first model reports approximately:

m_num_inputs  = 1
m_input_height = 640
m_input_width  = 640
m_input_channels = 3
m_sizeInBytes = 1228800

The second model reports:

m_num_inputs  = 1
m_input_height = 192
m_input_width = 192
m_input_channels = 3
m_sizeInBytes = 110592

I am sharing the tensor dimensions and memory requirements above.

------------------------------------------------------------
FAILURE
------------------------------------------------------------

When the custom application is started, libcamera configures:

(0) 760x568-RGB565
(1) 640x640-BGR888

Immediately afterwards the application terminates with:

terminate called after throwing an instance of 'std::bad_alloc' what(): std::bad_alloc

The kernel reports:

__vm_enough_memory: pid: ..., comm: queue2:src, not enough memory for the allocation

This makes me suspect that the second 640x640 camera stream, GStreamer queueing, DCMIPP buffers, or libcamera buffer allocation may be causing excessive memory allocation.

------------------------------------------------------------
PYTHON EXPERIMENT
------------------------------------------------------------

I also tried implementing the camera + STAI-MPU pipeline in Python 3.12.

In that implementation, libcamera negotiated:

(0) 800x600-BGR888
(1) 1280x1080-R8

The application then reported: appsink receiving 640x478 RGB

and immediately afterwards: Segmentation fault (core dumped)

This stream configuration is different from the official ST face-recognition application.

------------------------------------------------------------
CAMERA WARNINGS
------------------------------------------------------------

The following warnings are reported by libcamera:

'imx335 0-001a': Recommended V4L2 control 0x009a0922 not supported

'imx335 0-001a': The sensor kernel driver needs to be fixed

'imx335 0-001a': Failed to retrieve the camera location

'imx335 0-001a': Rotation control not available, default to 0 degrees

However, these warnings also appear when running the official ST face-recognition application, which works correctly.

Therefore, I am currently focusing on the difference in camera stream configuration and memory allocation.

------------------------------------------------------------
IMPORTANT COMPARISON
------------------------------------------------------------

                    Official ST       Custom application

Camera              IMX335             IMX335
Resolution           760x568            760x568
Source               LIBCAMERA          LIBCAMERA

Stream 0             760x568 RGB565     760x568 RGB565
Stream 1             128x128 BGR888     640x640 BGR888

Result               Works              std::bad_alloc

------------------------------------------------------------
QUESTIONS
------------------------------------------------------------

1. Is a 640x640 BGR888 secondary libcamera stream supported on STM32MP257F with the IMX335?

2. Is there a recommended maximum resolution for a secondary DCMIPP/libcamera stream?

3. Could the following error:

   __vm_enough_memory
   comm: queue2:src
   not enough memory for the allocation

   be caused by GStreamer queue buffers or libcamera/DCMIPP
   buffer allocation?

4. Are there specific buffer-count or queue-size settings that should be used for a 640x640 AI stream?

5. Is 640x640 BGR888 expected to require significantly more contiguous/video memory than the 128x128 BGR888 stream used
   by the official example?

6. For a custom STAI-MPU model with a 640x640 input, what is the recommended architecture?

   Option A:

       IMX335
          |
          +-- 760x568 camera stream
          |
          +-- 640x640 AI stream
                  |
                  +-- STAI-MPU

   or:

       IMX335
          |
          +-- 760x568 camera stream
                  |
                  +-- software resize/letterbox
                          |
                          +-- 640x640
                                  |
                                  +-- STAI-MPU

7. Is there an official ST recommendation for using custom 640x640 STAI-MPU models with libcamera on STM32MP257F?

8. Could the difference between the working ST application and my application be related to DMABUF, buffer stride, DCMIPP
   alignment, or GStreamer memory handling?

I can provide additional system information, camera format information, GStreamer pipeline information, dmesg output and application source code if required.

Thank you.