Skip to main content
Associate II
Aug 12, 2025 11:55 PM UTC
Solved

STM32MP257F-EV1 Tamper logging in Linux userspace

I'm trying to somehow pass information about tampering event from OP-TEE to Linux userspace by means of Tamper Backup registers but I seem to have a problem.

I added this to kernel dts:

&nvram {
	my_free_backup_register: tamp-bkp@c4 {
		reg = <0xC4 0x4>;
	};
};

&usart2 {
 // Other stuff before nvmem
	nvmem-cells = <&my_free_backup_register>;
	nvmem-cell-names = "my_backup_register"; 
};

I tried to write to that register from OP-TEE function stm32_tamp_etamper_action using io_write32 function. Then I'm trying to read that register from OP-TEE immediately after the write and looks like the register has not been written to.

Also, in Linux userspace in /sys/bus/nvmem/devices/ I can see stm32-tamp-nvram0 but when I hexdump its nvmem file it's just a bunch of zeroes. I can't seem to find that nvmem-cells in usart2 either.

This topic has been closed for replies.
rossUBest answer
Associate II
Aug 14, 2025 3:09 AM UTC

Ok, so looks like I wasn't able to write to TAMP_BKP49R because I had to first acknowledge tamper to unlock the register by clearing tamper flag in _TAMP_SCR. Then I was able to successfully write to it from OP-TEE and read from Linux with:

root@stm32mp2:~# hexdump -C /sys/bus/nvmem/devices/stm32-tamp-nvram0/nvmem

 

2 replies

Christophe Guibout
ST Technical Moderator
Aug 13, 2025 7:25 AM UTC

Hello @rossU,

 

You use TAMP_BKP49R, which is in Zone2 (Read Nonsecure/Write secure) : you should be  able to read it from the linux kernel: could you please detail how you read this tamper in linux ?

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
rossUAuthorBest answer
Associate II
Aug 14, 2025 3:09 AM UTC

Ok, so looks like I wasn't able to write to TAMP_BKP49R because I had to first acknowledge tamper to unlock the register by clearing tamper flag in _TAMP_SCR. Then I was able to successfully write to it from OP-TEE and read from Linux with:

root@stm32mp2:~# hexdump -C /sys/bus/nvmem/devices/stm32-tamp-nvram0/nvmem