Skip to main content
mfny
Associate II
Oct 13, 2024 10:34 AM UTC
Question

STM32MP257F-EV1 STLinux Packages: Serial command line

Hello,

I am wondering can the ST Linux Starter Package(or indeed any of the STLinux packages) be interacted with via a command line via serial port and if so how would this be set up ? as the additional display for this board is unavailable to me.

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
Oct 14, 2024 7:58 AM UTC

Hi @mfny 

for sure, the Starter Package console is available thru STLINK. This is the main control interface to Linux (for tests or install additional packages).

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-EV1/Let%27s_start/Unpack_the_STM32MP257x-EV1_board#Board_connections

Just connect USB Type-C CN21 to a PC and you will have 2 x VCP available (one for Cortex-A35 Console, the second optional for Cortex-M33 console).

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent