Skip to main content
Visitor II
Jul 15, 2026 2:20 PM UTC
Solved

STM32MP257F-DK - Using ST7789v with KMS DRM

Hello, I have a TFT LCD display that uses a ST7789v controller. I would like to interface with it using the KMS DRM subsystem in Linux. I have been having issues getting this to work though.

So far I have confirmed that the default driver to ST7789v controllers is running, but it only seems to create a drm_panel. I am having trouble creating/linking it to a connector/CRTC/encoder. I have any DBI related options enabled in menuconfig, but I don’t see any way to interface with DBI displays when running modetest. 

Does anyone have any advice as to what I need to do to get DRM working with this display? Will I need to write my own drivers? I can provide any existing code/devicetree configurations if need be.

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Jul 30, 2026 9:34 AM UTC

Hi ​@rpepe 

This question is now managed by AME local team through OLS

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Jul 30, 2026 9:34 AM UTC

Hi ​@rpepe 

This question is now managed by AME local team through OLS

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.