Skip to main content
jumman_JHINGA
Senior III
Jan 23, 2026 1:00 PM UTC
Solved

STM32MP257 OpenAMP RPMsg – Endpoint not getting created

Hi,

I’m working on STM32MP257F-DK (A35 + M33) using OpenAMP + RPMsg over IPCC and facing an issue with RPMsg endpoint creation on the M33 side.


Goal

Simple use case:

  • Linux (A35) sends "START" / "STOP"

  • M33 receives the message via RPMsg

  • M33 toggles an LED


What is working

  • M33 firmware builds and boots correctly using remoteproc

  • Resource table is detected

  • Virtio RPMsg is created on Linux

 

From Linux dmesg:

virtio_rpmsg_bus virtio0: rpmsg host is online
remoteproc remoteproc0: remote processor m33 is now up

So remoteproc and OpenAMP transport are working.


Problem

With the following M33 code, RPMsg endpoint is not getting created on Linux side:

int rpmsg_recv_callback(struct rpmsg_endpoint *ept,
 void *data,
 size_t len,
 uint32_t src,
 void *priv)
{
 if (len >= 5 && strncmp((char *)data, "START", 5) == 0)
 {
 led_run = 1;
 }
 else if (len >= 4 && strncmp((char *)data, "STOP", 4) == 0)
 {
 led_run = 0;
 HAL_GPIO_WritePin(GPIOZ, GPIO_PIN_0, GPIO_PIN_RESET);
 }

 return 0;
}

 struct rpmsg_device *rpmsg_dev;
// extern struct rpmsg_device *rpmsg_dev;
void OPENAMP_CreateEndpoint(void)
{
// if (!rpmsg_dev)
// {
// /* OpenAMP not ready yet */
// 	loc_printf("OpenAMP not ready yet.\r\n");
// return;
// }
	int status;
	status = rpmsg_create_ept(&rp_endpoint,
 rpmsg_dev,
 "rpmsg-led",
 RPMSG_ADDR_ANY,
 RPMSG_ADDR_ANY,
 rpmsg_recv_callback,
 NULL);
	if(status < 0){
		printf("End Point not created.\r\n");

		while(1){
			HAL_GPIO_TogglePin(GPIOZ, GPIO_PIN_0);
			 HAL_Delay(100);
		}
	}
}


/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* IPCC initialisation */
 MX_IPCC1_Init();

 if(!IS_DEVELOPER_BOOT_MODE())
 {
 /*Corpo Sync Initialization*/
	 CoproSync_Init();
 }
 /* OpenAmp initialisation ---------------------------------*/
 MX_OPENAMP_Init(RPMSG_REMOTE, NULL);

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 /* USER CODE BEGIN 2 */
 OPENAMP_CreateEndpoint();
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 OPENAMP_check_for_message();

 if (led_run)
 {
 HAL_GPIO_TogglePin(GPIOZ, GPIO_PIN_0);
 HAL_Delay(500);
 }
 else
 {
 HAL_Delay(10);
 }
 }
 /* USER CODE END 3 */
}

But:

rpmsg_create_ept() returns -1

Because of this:

  • Endpoint is not created on M33

  • Linux never sees or binds to the endpoint

  • No userspace RPMsg channel is available

  • M33 callback is never triggered


Linux side observation

/sys/class/rpmsg → only rpmsg_ctrl0
/dev → rpmsg0, rpmsg_ctrl0

 

  • No RPMsg data endpoint appears

  • /sys/class/rpmsg/rpmsg_ctrl0/new_endpoint → permission denied

  • /dev/ttyRPMSG* does not exist

Any guidance or reference example for STM32MP257 RPMsg endpoint creation on M33 would be very helpful.

Thanks.

 

Bernard PUEL
Bernard PUELBest answer
ST Technical Moderator
Feb 2, 2026 2:12 PM UTC

Hello,

you can have a look here to better trace what happens = https://wiki.st.com/stm32mpu/wiki/Cortex-M_remote_processor_management_troubleshooting_grid

 

To get better understanding of the architecture = https://wiki.st.com/stm32mpu/wiki/Interprocessor_communication_%E2%80%93_exchanging_buffers

 

This article will give you all the details of current example based on openAMP, you can get as reference = https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-DK/Develop_on_Arm_Cortex-M33/Modify,_rebuild_and_reload_the_firmware

 

Hope it will help !!

 

 

1 reply

Bernard PUEL
Bernard PUELBest answer
ST Technical Moderator
Feb 2, 2026 2:12 PM UTC

Hello,

you can have a look here to better trace what happens = https://wiki.st.com/stm32mpu/wiki/Cortex-M_remote_processor_management_troubleshooting_grid

 

To get better understanding of the architecture = https://wiki.st.com/stm32mpu/wiki/Interprocessor_communication_%E2%80%93_exchanging_buffers

 

This article will give you all the details of current example based on openAMP, you can get as reference = https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-DK/Develop_on_Arm_Cortex-M33/Modify,_rebuild_and_reload_the_firmware

 

Hope it will help !!