Skip to main content
Associate
Aug 21, 2026 7:06 AM UTC
Solved

STM32MP23x Multi-Stream CSI-2 Four-Camera Support

Can the STM32MP231 simultaneously capture or stream four 2-lane MIPI CSI-2 camera streams through a DS90UB960/TDES960 using VC0–VC3?

I have reviewed ST’s documentation on “How to use one or multiple multi-stream MIPI CSI cameras.” But did not get complete clarity on simultaneous capture of four camera streams. The documentation example appears to show routing for up to three streams/channels through the DCMIPP pipes (Dump, Main, and Aux).

Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
Aug 21, 2026 9:35 AM UTC

Hello ​@Jiwesh ,
Today we support up to 1 VC per DCMIPP pipeline, so yes you are right, the maximum number of Virtual Channel the DCMIPP can handle is 3 (for Dump, Main and Aux).


Just for your information. In theory (from a HW point of view), there is a possibility that 1 single pipeline entry support 2 different VC, by “flip flopping” the VC configured in the Input selector to change at each frame (and so by dividing by 2 the framerate of each flow). However the SW does not support it today and there is no plan to develop it short term.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

3 replies

Erwan SZYMANSKI
Erwan SZYMANSKIBest answer
ST Technical Moderator
Aug 21, 2026 9:35 AM UTC

Hello ​@Jiwesh ,
Today we support up to 1 VC per DCMIPP pipeline, so yes you are right, the maximum number of Virtual Channel the DCMIPP can handle is 3 (for Dump, Main and Aux).


Just for your information. In theory (from a HW point of view), there is a possibility that 1 single pipeline entry support 2 different VC, by “flip flopping” the VC configured in the Input selector to change at each frame (and so by dividing by 2 the framerate of each flow). However the SW does not support it today and there is no plan to develop it short term.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JiweshAuthor
Associate
Sep 9, 2026 10:19 AM UTC

Thanks for the clarification, Erwan!

JiweshAuthor
Associate
Sep 9, 2026 10:17 AM UTC

.