Skip to main content
MWoło.2
Senior III
May 12, 2022 9:00 AM UTC
Solved

Stm32mp1xxx uart4 U-Boot stop boot routine when the Stlink not connected

Hi,

I have a small problem during stm32mp1xxx bring up. The Uart4 is debug console and is connected to stlink v2.1 on virtual serial. The problem is that this stlink makes all the time interrupt U-Boot and stack in it (stlink not connected to USB). To go system father I need to connect stlink to USB and type 'boot'.

I tried to add

CONFIG_BOOTDELAY=-2
CONFIG_SILENT_CONSOLE=y
CONFIG_SYS_DEVICE_NULLDEV=y
CONFIG_SILENT_CONSOLE_UPDATE_ON_SET=y
CONFIG_SILENT_U_BOOT_ONLY=y

but without success.

In the hardware, I added pull up resistors

0693W00000NpphUQAR.pngTo prove my theory I make a shortcut on resistor R58 and the system boot-up all the time.

How to correctly resolve this problem

Thanks in advanced

BR Michal

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
May 12, 2022 9:35 AM UTC

Hi @Michał Wołowik​ ,

Similar behavior has been seen on some rather old ST-Link FW versions (V2J33M25 if I remember).

Please update to latest FW : https://www.st.com/en/development-tools/stsw-link007.html

Regards

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

2 replies

PatrickF
PatrickFBest answer
ST Employee
May 12, 2022 9:35 AM UTC

Hi @Michał Wołowik​ ,

Similar behavior has been seen on some rather old ST-Link FW versions (V2J33M25 if I remember).

Please update to latest FW : https://www.st.com/en/development-tools/stsw-link007.html

Regards

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
MWoło.2
MWoło.2Author
Senior III
May 12, 2022 11:57 AM UTC

Perfect answer as always ;)

Thanks, Patrick, of course working after upgrading to the latest.

BR Michal