stm32mp157f-dk2 usb gadget
- 3 replies
- 5097 views
Hi everyone,
I am using stm32mp157f-dk2 with ecosystem 3.1.
I want to configure the usb type C port(CN7) as serial port, and communicate with the host PC.
This article helps me a lot. https://wiki.st.com/stm32mpu/wiki/USB_overview#How_to_configure_USB_Gadget_through_configfs
I modified the usbotg-gadget-config.bb, the stm32_usbotg_eth_config.sh and create my own service, as attached.
After that, I can successfully set up the device. I can see ttyGS0 show up in my device.
However, when I connect it to the host, although the host is able to detect my device, it can't recognize my device.
What am I missing?
I suspect that it is the stlink causing the issue, as it occupy the ttyACM0 already and the host cannot create another tty corresponding to the GS0. I am not sure how will the host OS deal with this situation.
Regards,
Leung
10/3 update: I found that my PC can't boot up when the device is connected. It scared me. I am still investigating why it is failing, but I think the stlink is not the root cause.