Skip to main content
asadullah4571
Associate III
Aug 30, 2024 6:01 AM UTC
Question

STM32MP157f-dk2 PWM input pin

Hi Every One 

i am facing the issue to find the pins of PWM in the (STM32mp157f-dk2 ), i configured the PWM channel in device tree and pwm channel is visible in  /sys/class/pemchip0/pwm , so i need to collect the input from the pins but which pin is connected to PWM i do not know , could you please help me out this.

(this is my my output form the board terminal )
root@stm32mp1:/sys/class/pwm/pwmchip0/pwm0# ls
capture duty_cycle enable period polarity power uevent
root@stm32mp1:/sys/class/pwm/pwmchip0/pwm0#

I Need 
1. how to use pin and which pin i  need to connect 

2. i want to collect the input prom the PWM.
3. and the should be show on the terminal. 

if i am wrong and any thing missing , please correct me 

This topic has been closed for replies.