Skip to main content
Associate II
Feb 20, 2026 10:06 AM UTC
Question

Stm32mp157c-odyssey OTG issues

Hello, 
I am using and stm32mp157c-odyssey SoM with a custom made motherboard, 
However I am having issues getting the usb port function properly.I am using otg fs. It fails the enumeration in the pc side and gets stuck at L1 sometimes and other errors. I still don't know if it's a hardware or software related issues. I am configuring it as device only. 
below I will include picture of the usb schematic, the logs, as well as the device tree node.
 Note : We are not using otg_fs_id it's not connected to anythhing , and vbus comes directly from the PC host to the OTG_vbus pin so no vbus gpio.
Using yocto image 6.1 mickledore.

&usbotg_hs {
compatible = "st,stm32mp15-fsotg", "snps,dwc2";
status = "okay";

pinctrl-names = "default";
pinctrl-0 = <&usbotg_fs_dp_dm_pins_a>;
dr_mode = "peripheral";

};

4 replies

ST Technical Moderator
Feb 23, 2026 11:42 AM UTC

Hi @softcity002 

It seems control transfers on EP0 are failing. Disable LPM as a test.

This could be SW or hardware issue. You can reach to Seeed SoM directly to get support.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate II
Feb 24, 2026 6:33 AM UTC

Hello, I did disable LPM but the behavior didn't change.

PatrickF
ST Employee
Feb 23, 2026 4:39 PM UTC

Hi, 

 

did you try to use similar settings than the high-speed without VBUS nor ID ?
DT configuration example as high-speed OTG in Host or Peripheral mode, with micro-B or Type-C connector, and with VBUS and ID left unconnected

	dr_mode = "peripheral"; 
	usb-role-switch; 
	role-switch-default-mode = "peripheral"; 

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Associate II
Feb 24, 2026 6:35 AM UTC

Hi.

I did try that and everything proposed in the ST wiki, but same behavior.