Skip to main content
Associate II
Jun 23, 2023 9:40 AM UTC
Solved

STM32MP157C Enabling usart1 by using device tree

Hi all,

The development board we are using STM32MP157C-YA157C from Myirtech is running Ubuntu 18 with openstlinux.

I am trying to interface the usart1 with another module but by default, the peripheral is not enabled from device tree.

So, I modified the device tree as follows (pins z6 and z7 are used by usart1) according to the document of ST :

 

 

 

usart1_pins_a: usart1-0 {
pins1 {
pinmux = <STM32_PINMUX('Z', 7, AF7)>; /* UART1_TX */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
pins2 {
pinmux = <STM32_PINMUX('Z', 6, AF7)>; /* UART1_RX */
bias-disable;
};
};

usart1_idle_pins_a: usart1-idle-0 {
pins1 {
pinmux = <STM32_PINMUX('Z', 7, ANALOG)>; /* UART1_TX */
};
pins2 {
pinmux = <STM32_PINMUX('Z', 6, AF7)>; /* UART1_RX */
bias-disable;
};
};

usart1_sleep_pins_a: usart1-sleep-0 {
pins {
pinmux = <STM32_PINMUX('Z', 7, ANALOG)>, /* UART1_TX */
<STM32_PINMUX('Z', 6, ANALOG)>; /* UART1_RX */
};
};
&usart1 {
	pinctrl-names = "default", "sleep", "idle";	/* pin configurations definition */
	pinctrl-0 = <&usart1_pins_a>;			/* default pin configuration selection */
	pinctrl-1 = <&usart1_sleep_pins_a>;		/* sleep pin configuration selection */
	pinctrl-2 = <&usart1_idle_pins_a>;		/* idle pin configuration selection */
	status = "okay";				/* device activation */
};
aliases {
		ethernet0 = &ethernet0;
		serial0 = &uart4;
		serial1 = &usart1;
		serial2 = &uart8;//rs232
		serial3 = &uart5;//rs485
		serial4 = &uart7;//bt
	};
usart1: serial@5c000000 {
			compatible = "st,stm32h7-uart";
			reg = <0x5c000000 0x400>;
			interrupts-extended = <&exti 26 IRQ_TYPE_LEVEL_HIGH>;
			//clocks = <&scmi0_clk CK_SCMI0_USART1>;
			//resets = <&scmi0_reset RST_SCMI0_USART1>;
			clocks = <&rcc USART1_K>;
			resets = <&rcc USART1_R>;
			
			wakeup-source;
			power-domains = <&pd_core>;
			status = "disabled";
		};

 

 

 

On boot up, the kernel cannot enable the usart1 module (5c000000):

 

 

 

[ 1.961813] stm32-usart 40010000.serial: interrupt mode for rx (no dma)
[ 1.961838] stm32-usart 40010000.serial: interrupt mode for tx (no dma)
[ 1.961877] 40010000.serial: ttySTM0 at MMIO 0x40010000 (irq = 57, base_baud = 4000000) is a stm32-usart
[ 3.239179] 40011000.serial: ttySTM3 at MMIO 0x40011000 (irq = 58, base_baud = 4000000) is a stm32-usart
[ 3.249682] 40018000.serial: ttySTM4 at MMIO 0x40018000 (irq = 59, base_baud = 4000000) is a stm32-usart
[ 3.264333] 40019000.serial: ttySTM2 at MMIO 0x40019000 (irq = 60, base_baud = 4000000) is a stm32-usart
[ 3.279710] stm32-usart: probe of 5c000000.serial failed with error -22

 

 

 

 The clock summary is as follows (grep -E "clock|usart" /sys/kernel/debug/clk/clk_summary | sed 's,\s\+, ,g' | column -t):

 

 

 

clock count count count rate accuracy phase cycle
usart1_k 0 0 0 64000000 0 0 50000
usart3_k 0 0 0 64000000 0 0 50000
usart2_k 0 0 0 64000000 0 0 50000
usart6 0 0 0 104438965 0 0 50000
usart3 0 0 0 104438965 0 0 50000
usart2 0 0 0 104438965 0 0 50000

 

 

 

I noticed that the usart1_k  clock is not enabled. How can I enable it?
What am I missing?

Thank you.

Best regards,

Mert

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Jun 26, 2023 9:44 AM UTC

Hi @mertt 

I think it miss to enable  and provide a source clock to UART1 clock in Tf-a Device Tree 

st,pkcs = <
...
CLK_UART1_DISABLED

CLK_UART1_HSI
...
>;

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

5 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Jun 26, 2023 9:44 AM UTC

Hi @mertt 

I think it miss to enable  and provide a source clock to UART1 clock in Tf-a Device Tree 

st,pkcs = <
...
CLK_UART1_DISABLED

CLK_UART1_HSI
...
>;

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
merttAuthor
Associate II
Jun 26, 2023 11:37 AM UTC

Hi @Olivier GALLIEN 

Thank you for the answer.

In the file include/dt-bindings/clock/stm32mp1-clks.h, there are the following definitions:

#define USART1 64
...
#define CK_SCMI0_HSI 1
...
#define CK_SCMI0_USART1 20

I suspect that the kernel versions are different.

Under the rcc: rcc@50000000, I can use the following, if it is correct:

st,pkcs = <
...
CK_SCMI0_USART1
...
>;

 

Best regards,
Mert

merttAuthor
Associate II
Jun 26, 2023 12:25 PM UTC

> I think it miss to enable  and provide a source clock to UART1 clock in Tf-a Device Tree 

I missed the tf-a part, I will try to compile and change the boot partition again.

Best regards.

merttAuthor
Associate II
Jul 2, 2023 6:55 AM UTC

It worked, thanks.


[3.270418] 5c000000.serial: ttySTM1 at MMIO 0x5c000000 (irq = 61, base_baud = 4000000) is a stm32-usart