Skip to main content
Visitor II
Dec 1, 2024 12:52 AM UTC
Question

STM32MP157 processor and OpenAMP

Hello i have STM32MP157 board with A7 and M4 processors, i am trying to setup OpenAMP which works when i use the OpenAMP_TTY_echo
But when i try to create a new project from:

SMT32Cube IDE 1.16.0 version

STM32MP1 version: 1.6.0

I cannot seem to make it work

For example, when i deploy the example it properly opens the port /dev/ttyRPMSG0 and when i read with this command cat /dev/ttyRPMSG0 it wait for messages , so i connect to another temrinal send some messages and receive them perfectly

But when i try to use generated project the port is not even open and this is my output of the rpmsg0 :

[ 1.668065] rpmsg_sdb_drv_init(rpmsg_sdb): Init done
[ 40.830549] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty addr 0x400
[ 40.837511] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty addr 0x401
[ 40.848325] virtio_rpmsg_bus virtio0: rpmsg host is online

Looks good , also when starting the processor:

root@myir:~# dmesg | grep remoteproc
[ 1.667805] remoteproc remoteproc0: releasing m4
[ 1.749203] remoteproc remoteproc0: releasing m4
[ 1.788187] remoteproc remoteproc0: releasing m4
[ 1.923612] remoteproc remoteproc0: releasing m4
[ 4.222566] remoteproc remoteproc0: m4 is available
[ 40.754770] remoteproc remoteproc0: powering up m4
[ 40.797573] remoteproc remoteproc0: Booting fw image rproc-m4-fw, size 2443240
[ 40.865267] remoteproc remoteproc0: remote processor m4 is now up

I am not sure what i am doing wrong
This is my code

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "openamp.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <string.h>
#include <virt_uart.h>
#include <ctype.h> // For character transformations like toupper

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define MAX_BUFFER_SIZE RPMSG_BUFFER_SIZE

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
IPCC_HandleTypeDef hipcc;

/* USER CODE BEGIN PV */
VIRT_UART_HandleTypeDef huart0;
VIRT_UART_HandleTypeDef huart1;

__IO FlagStatus VirtUart0RxMsg = RESET;
uint8_t VirtUart0ChannelBuffRx[MAX_BUFFER_SIZE];
uint16_t VirtUart0ChannelRxSize = 0;

__IO FlagStatus VirtUart1RxMsg = RESET;
uint8_t VirtUart1ChannelBuffRx[MAX_BUFFER_SIZE];
uint16_t VirtUart1ChannelRxSize = 0;

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_IPCC_Init(void);
int MX_OPENAMP_Init(int RPMsgRole, rpmsg_ns_bind_cb ns_bind_cb);
/* USER CODE BEGIN PFP */
void VIRT_UART0_RxCpltCallback(VIRT_UART_HandleTypeDef *huart);
void VIRT_UART1_RxCpltCallback(VIRT_UART_HandleTypeDef *huart);
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initialize the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */
 if(IS_ENGINEERING_BOOT_MODE())
 {
 /* Configure the system clock */
 SystemClock_Config();
 }


 /* USER CODE END Init */

 /*HW semaphore Clock enable*/
 __HAL_RCC_HSEM_CLK_ENABLE();
 /* IPCC initialisation */
 MX_IPCC_Init();
 MX_OPENAMP_Init(RPMSG_REMOTE, NULL);
 /* OpenAmp initialisation ---------------------------------*/


 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 /* USER CODE BEGIN 2 */
 /*
 * Create Virtual UART device
 * defined by a rpmsg channel attached to the remote device
 */

 if (VIRT_UART_Init(&huart0) != VIRT_UART_OK) {

 Error_Handler();
 }


 if (VIRT_UART_Init(&huart1) != VIRT_UART_OK) {

 Error_Handler();
 }

 /*Need to register callback for message reception by channels*/
 if(VIRT_UART_RegisterCallback(&huart0, VIRT_UART_RXCPLT_CB_ID, VIRT_UART0_RxCpltCallback) != VIRT_UART_OK)
 {
 Error_Handler();
 }
 if(VIRT_UART_RegisterCallback(&huart1, VIRT_UART_RXCPLT_CB_ID, VIRT_UART1_RxCpltCallback) != VIRT_UART_OK)
 {
 Error_Handler();
 }
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {

 OPENAMP_check_for_message();

 /* USER CODE END WHILE */

 if (VirtUart0RxMsg)
 {
 VirtUart0RxMsg = RESET;
 VIRT_UART_Transmit(&huart0, VirtUart0ChannelBuffRx, VirtUart0ChannelRxSize);
 }

 if (VirtUart1RxMsg) {
 VirtUart1RxMsg = RESET;
 VIRT_UART_Transmit(&huart1, VirtUart1ChannelBuffRx, VirtUart1ChannelRxSize);
 }
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSIDivValue = RCC_HSI_DIV1;
 RCC_OscInitStruct.LSIState = RCC_LSI_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_NONE;
 RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_NONE;
 RCC_OscInitStruct.PLL4.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** RCC Clock Config
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_ACLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3|RCC_CLOCKTYPE_PCLK4
 |RCC_CLOCKTYPE_PCLK5;
 RCC_ClkInitStruct.AXISSInit.AXI_Clock = RCC_AXISSOURCE_HSI;
 RCC_ClkInitStruct.AXISSInit.AXI_Div = RCC_AXI_DIV1;
 RCC_ClkInitStruct.MCUInit.MCU_Clock = RCC_MCUSSOURCE_HSI;
 RCC_ClkInitStruct.MCUInit.MCU_Div = RCC_MCU_DIV1;
 RCC_ClkInitStruct.APB4_Div = RCC_APB4_DIV1;
 RCC_ClkInitStruct.APB5_Div = RCC_APB5_DIV1;
 RCC_ClkInitStruct.APB1_Div = RCC_APB1_DIV1;
 RCC_ClkInitStruct.APB2_Div = RCC_APB2_DIV1;
 RCC_ClkInitStruct.APB3_Div = RCC_APB3_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief IPCC Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_IPCC_Init(void)
{

 /* USER CODE BEGIN IPCC_Init 0 */

 /* USER CODE END IPCC_Init 0 */

 /* USER CODE BEGIN IPCC_Init 1 */

 /* USER CODE END IPCC_Init 1 */
 hipcc.Instance = IPCC;
 if (HAL_IPCC_Init(&hipcc) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN IPCC_Init 2 */

 /* USER CODE END IPCC_Init 2 */

}

/* USER CODE BEGIN 4 */


void VIRT_UART0_RxCpltCallback(VIRT_UART_HandleTypeDef *huart)
{
 uint16_t total_len;
 const char *response;

 // Ensure the received message is null-terminated
 uint16_t received_size = (huart->RxXferSize < MAX_BUFFER_SIZE - 1) ? huart->RxXferSize : MAX_BUFFER_SIZE - 2;
 memcpy(VirtUart0ChannelBuffRx, huart->pRxBuffPtr, received_size);
 VirtUart0ChannelBuffRx[received_size] = '\0'; // Null-terminate

 // Trim trailing whitespace and control characters
 while (received_size > 0 &&
 (VirtUart0ChannelBuffRx[received_size - 1] == '\n' ||
 VirtUart0ChannelBuffRx[received_size - 1] == '\r' ||
 VirtUart0ChannelBuffRx[received_size - 1] == ' ' ||
 VirtUart0ChannelBuffRx[received_size - 1] == '\t')) {
 VirtUart0ChannelBuffRx[received_size - 1] = '\0';
 received_size--;
 }


 // Check the received message and set the response
 if (strcmp((char *)VirtUart0ChannelBuffRx, "ledon") == 0)
 {
 response = "The LED is on";
 }
 else if (strcmp((char *)VirtUart0ChannelBuffRx, "ledoff") == 0)
 {
 response = "The LED is off";
 }
 else
 {
 response = "Unknown command";
 }

 // Copy the response into the buffer
 total_len = strlen(response);
 if (total_len >= MAX_BUFFER_SIZE)
 {
 total_len = MAX_BUFFER_SIZE - 1;
 }
 memcpy(VirtUart0ChannelBuffRx, response, total_len);
 VirtUart0ChannelBuffRx[total_len] = '\0'; // Null-terminate

 // Update the size for transmission
 VirtUart0ChannelRxSize = total_len;

 VirtUart0RxMsg = SET;
}





void VIRT_UART1_RxCpltCallback(VIRT_UART_HandleTypeDef *huart)
{


 /* copy received msg in a variable to sent it back to master processor in main infinite loop*/
 VirtUart1ChannelRxSize = huart->RxXferSize < MAX_BUFFER_SIZE? huart->RxXferSize : MAX_BUFFER_SIZE-1;
 memcpy(VirtUart1ChannelBuffRx, huart->pRxBuffPtr, VirtUart1ChannelRxSize);
 VirtUart1RxMsg = SET;
}

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 


I searched the internet but with no luck , not sure what i am missing

 

If somebody could help

Thank you

 

This topic has been closed for replies.