Skip to main content
Associate III
Jun 27, 2024 9:11 AM UTC
Question

STM32MP157 FIRMWARE

I developed a new stm32mp157 board. Do I need to update the firmware to run A7 on stm32mp157? Or is the firmware already updated?

This topic has been closed for replies.

3 replies

Olivier GALLIEN
ST Technical Moderator
Jun 28, 2024 12:20 PM UTC

Hi @LeeJaewon ,

 

Sorry I don't understand the question.

Did you refer to : stm32mpu 

 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
LeeJaewonAuthor
Associate III
Jul 1, 2024 1:50 AM UTC

I'm talking about the stm32mp157fac chip.

 

Do users need to separately upload firmware to run the A7 core?

Or, I would like to know if it was already done at the time of production.

 

I created the circuit and artwork to match the stm32mp157 discovery board.

Associate II
Jul 1, 2024 7:17 AM UTC

STM32MP15x MPUs does not come with an embedded flash memory, that is why you need to incorporate uSD card, eMMC or NAND/NOR flash on your custom board.

Only basic boot functionalities are integrated by ST inside the chip, the rest of the boot sequence and user application must be flashed on an external memory, such as the uSD card you can find in discovery kits.