Skip to main content
Associate II
Aug 19, 2024 4:31 PM UTC
Solved

STM32MP157-EV1 Display not working on first boot

I'm trying to get STM32MP157F-EV1 board working with the STM32Cube ecosystem.  I have successfully followed the getting started guide., STM32MP157x-EV1 Lets Start   URL.  I get to the last step in  /Populate_the_target_and_boot_the_image, (Step 8), Boot the Board and GUI never shows up on Display.   After multiple reboots, reflashes, I thought let me go to next step, anyways, https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-EV1/Let%27s_start/Execute_basic_commands .  Well it turns out that I am able to login to device using Minicom.  I checked dmesg output, 

dmesg | grep display
[ 0.117034] platform 5a001000.display-controller: Fixed dependency cycle(s) with /soc/dsi@5a000000
[ 0.131004] platform 5a001000.display-controller: Fixed dependency cycle(s) with /soc/dsi@5a000000
[ 0.131240] platform 5a000000.dsi: Fixed dependency cycle(s) with /soc/display-controller@5a001000
[ 2.751026] stm32-display-dsi 5a000000.dsi: Fixed dependency cycle(s) with /soc/dsi@5a000000/panel-dsi@0
[ 2.863569] [drm] Initialized stm 1.0.0 20170330 for 5a001000.display-controller on minor 0
[ 19.592612] stm32-display-dsi 5a000000.dsi: Timeout during read operation
[ 35.242363] stm32-display-dsi 5a000000.dsi: Timeout during read operatio

I am wondering if I am doing a step incorrectly, but I just follwed the Guide.  So wondering if  a) Documentation is incorrect, or b) my HW display is bad.

Demo Launcher does not display.

Using, Create a simple Hello World program application I am able to compile "Hello World" program but it too, does not display a UI on STM32MP157F-ev1

Where else can I look for HW display not working or what additional information is needed to troubleshoot?

 

 

 

This topic has been closed for replies.
pme991Best answer
Associate II
Sep 6, 2024 5:01 PM UTC

@Erwan SZYMANSKI ,

 

This issue is resolved on my end.  Turns out one of the boards was  loose, and not set properly.  After I removed board (power goes into)  and reseated it on the board, the display work properly.

 

Thanks

5 replies

Erwan SZYMANSKI
ST Technical Moderator
Aug 20, 2024 8:54 AM UTC

Hello @pme991 ,
Can you attach the complete boot logs of your board, as well as a picture of your setup ?

Do you at least see a back-light on your screen or is it completely black without any sign of life ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
pme991Author
Associate II
Aug 21, 2024 1:23 AM UTC

@Erwan SZYMANSKI 

Let me know the location of the boot log you wish to view, I am happy to provide, I am attaching output from dmesg.  Here is picture of my board, all LED seems to be functioning.  Display is dark, I don't believe it is backlit.

 

20240820_180412.jpg

pme991Author
Associate II
Aug 21, 2024 1:36 AM UTC

@Erwan SZYMANSKI 

Some additional info, in dmesg output (dmesg.txt) I see this failure:

 

[ 2.915285] stmfx-core 0-0042: Boot chip failed: -6
[ 2.918782] ------------[ cut here ]------------
[ 2.920871] mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11
[ 2.923421] WARNING: CPU: 1 PID: 47 at drivers/regulator/core.c:2403 _regulator_put+0x15c/0x164
[ 2.937426] Modules linked in:
[ 2.940387] CPU: 1 PID: 47 Comm: kworker/u4:4 Not tainted 6.1.82 #1
[ 2.946658] Hardware name: STM32 (Device Tree Support)
[ 2.951816] Workqueue: events_unbound deferred_probe_work_func
[ 2.957608] unwind_backtrace from show_stack+0x10/0x14

Here is output file from "journalctl -xb" 

 

Erwan SZYMANSKI
ST Technical Moderator
Aug 21, 2024 11:53 AM UTC

Hello @pme991 ,
For sure there is a communication problem with your display, we can clearly see it thanks to following logs in  your dmesg.txt : 

[ 19.192278] stm32-display-dsi 5a000000.dsi: Timeout during read operation
[ 19.197685] panel-rocktech-hx8394 5a000000.dsi.0: could not read MTP ID1

As you say that you only took the Starter Package, I will check internally if we had a similar case in our test farm. If not, we can consider an HW issue with the DSI panel.

I will let you informed ASAP.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
pme991AuthorBest answer
Associate II
Sep 6, 2024 5:01 PM UTC

@Erwan SZYMANSKI ,

 

This issue is resolved on my end.  Turns out one of the boards was  loose, and not set properly.  After I removed board (power goes into)  and reseated it on the board, the display work properly.

 

Thanks