Visitor II
Jun 20, 2025 12:03 PM UTC
Question
STM32MP135 custom board emmc boot error (userfs doesn't exist)
- 1 reply
- 292 views
Hello.
I have a custom stm32mp135f board with emmc1(SDMMC2) and about to launch linux.
(Minimized version of 135f-dk, no-sdcard, no-ethernet)
I flashed the target with the CubeProgrammer normally.
When the kernel loads userfs there says 'root '/dev/disk/by-partuuid/491f6117-415d-4f53-88c9-6e0de54deac6' doesn't exist or does not contain a /dev." and stopped.
How do I solve this problem?
This is full log capture.
Starting kernel ...
I/TC: Reserved shared memory is disabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are enabled
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 6.6.48-gd96ac4cc57f6 (oe-user@oe-host) (arm-ostl-linux-gnueabi-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240716) #1 PREEMPT Fri Jun 20 08:08:22 UTC 2025
[ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: STMicroelectronics STM32MP135F-DK STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] OF: reserved mem: 0xdd000000..0xdfffffff (49152 KiB) nomap non-reusable optee@dd000000
[ 0.000000] cma: Reserved 64 MiB at 0xd9000000 on node -1
[ 0.000000] Zone ranges:
[ 0.000000] Normal [mem 0x00000000c0000000-0x00000000dcffffff]
[ 0.000000] HighMem [mem 0x00000000dd000000-0x00000000dfffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x00000000c0000000-0x00000000dcffffff]
[ 0.000000] node 0: [mem 0x00000000dd000000-0x00000000dfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x00000000c0000000-0x00000000dfffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.0 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] Kernel command line: root=PARTUUID=491f6117-415d-4f53-88c9-6e0de54deac6 rootwait rw console=ttySTM0,115200
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes, linear)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 130028
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] Memory: 376784K/524288K available (13312K kernel code, 1416K rwdata, 3968K rodata, 1024K init, 220K bss, 81968K reserved, 65536K cma-reserved, 0K highmem)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] trace event string verifier disabled
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (virt).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns
[ 0.000001] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns
[ 0.000017] Switching to timer-based delay loop, resolution 41ns
[ 0.000731] Console: colour dummy device 80x30
[ 0.000782] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)
[ 0.000802] CPU: Testing write buffer coherency: ok
[ 0.000866] pid_max: default: 32768 minimum: 301
[ 0.001073] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.001100] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.004260] RCU Tasks: Setting shift to 0 and lim to 1 rcu_task_cb_adjust=1.
[ 0.004473] RCU Tasks Trace: Setting shift to 0 and lim to 1 rcu_task_cb_adjust=1.
[ 0.004697] Setting up static identity map for 0xc0100000 - 0xc0100060
[ 0.004957] rcu: Hierarchical SRCU implementation.
[ 0.004971] rcu: Max phase no-delay instances is 1000.
[ 0.006703] devtmpfs: initialized
[ 0.020020] VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
[ 0.020394] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.020437] futex hash table entries: 256 (order: -1, 3072 bytes, linear)
[ 0.023491] pinctrl core: initialized pinctrl subsystem
[ 0.026267] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.030093] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.031627] thermal_sys: Registered thermal governor 'step_wise'
[ 0.031762] cpuidle: using governor menu
[ 0.032068] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.032086] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.032639] Serial: AMBA PL011 UART driver
[ 0.035541] stm32-pm-domain pm_domain: domain core-ret-power-domain registered
[ 0.035580] stm32-pm-domain pm_domain: subdomain core-power-domain registered
[ 0.035591] stm32-pm-domain pm_domain: domains probed
[ 0.053202] kprobes: kprobe jump-optimization is enabled. All kprobes are optimized if possible.
[ 0.066633] SCSI subsystem initialized
[ 0.070744] usbcore: registered new interface driver usbfs
[ 0.070804] usbcore: registered new interface driver hub
[ 0.070891] usbcore: registered new device driver usb
[ 0.071363] pps_core: LinuxPPS API ver. 1 registered
[ 0.071377] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.071403] PTP clock support registered
[ 0.071836] EDAC MC: Ver: 3.0.0
[ 0.080796] scmi_core: SCMI protocol bus registered
[ 0.084092] clocksource: Switched to clocksource arch_sys_counter
[ 0.116306] NET: Registered PF_INET protocol family
[ 0.116649] IP idents hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.124574] tcp_listen_portaddr_hash hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.124627] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.124671] TCP established hash table entries: 4096 (order: 2, 16384 bytes, linear)
[ 0.124718] TCP bind hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.124794] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.124926] UDP hash table entries: 256 (order: 0, 4096 bytes, linear)
[ 0.124963] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes, linear)
[ 0.125273] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.126312] RPC: Registered named UNIX socket transport module.
[ 0.126336] RPC: Registered udp transport module.
[ 0.126342] RPC: Registered tcp transport module.
[ 0.126346] RPC: Registered tcp-with-tls transport module.
[ 0.126349] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.126871] hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available
[ 0.128897] Initialise system trusted keyrings
[ 0.129875] Trying to unpack rootfs image as initramfs...
[ 0.144247] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 0.144858] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.145617] NFS: Registering the id_resolver key type
[ 0.145702] Key type id_resolver registered
[ 0.145713] Key type id_legacy registered
[ 0.145783] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.145796] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.145866] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.145908] jffs2: version 2.2. (NAND) ⓒ 2001-2006 Red Hat, Inc.
[ 0.154348] fuse: init (API version 7.39)
[ 0.155211] NET: Registered PF_ALG protocol family
[ 0.155241] Key type asymmetric registered
[ 0.155250] Asymmetric key parser 'x509' registered
[ 0.155372] bounce: pool size: 64 pages
[ 0.155460] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 0.155472] io scheduler mq-deadline registered
[ 0.155480] io scheduler kyber registered
[ 0.155554] io scheduler bfq registered
[ 0.155883] /soc/interrupt-controller@5000d000: bank0
[ 0.155920] /soc/interrupt-controller@5000d000: bank1
[ 0.155935] /soc/interrupt-controller@5000d000: bank2
[ 0.156898] Registering stm32-etzpc firewall controller
[ 0.187702] STM32 USART driver initialized
[ 0.249796] brd: module loaded
[ 0.279847] loop: module loaded
[ 0.307755] CAN device driver interface
[ 0.309318] pegasus: Pegasus/Pegasus II USB Ethernet driver
[ 0.309404] usbcore: registered new interface driver pegasus
[ 0.309465] usbcore: registered new interface driver asix
[ 0.309517] usbcore: registered new interface driver ax88179_178a
[ 0.309562] usbcore: registered new interface driver cdc_ether
[ 0.309607] usbcore: registered new interface driver smsc75xx
[ 0.309655] usbcore: registered new interface driver smsc95xx
[ 0.309699] usbcore: registered new interface driver net1080
[ 0.309752] usbcore: registered new interface driver cdc_subset
[ 0.309798] usbcore: registered new interface driver zaurus
[ 0.309897] usbcore: registered new interface driver cdc_ncm
[ 0.311916] usbcore: registered new interface driver usb-storage
[ 0.312182] usbcore: registered new device driver onboard-usb-hub
[ 0.335898] i2c_dev: i2c /dev entries driver
[ 0.339462] arm_smc_wdt watchdog: Watchdog registered (timeout=32 sec, nowayout=0)
[ 0.340575] stm32-cpufreq stm32-cpufreq: OPP-v2 not supported
[ 0.341520] sdhci: Secure Digital Host Controller Interface driver
[ 0.341535] sdhci: Copyright(c) Pierre Ossman
[ 0.341542] Synopsys Designware Multimedia Card Interface Driver
[ 0.341907] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.342679] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.343546] usbcore: registered new interface driver usbhid
[ 0.343564] usbhid: USB HID core driver
[ 0.367279] optee: probing for conduit method.
[ 0.367319] optee: revision 4.0 (2a5b1d12)
[ 0.424654] optee: Asynchronous notifications enabled
[ 0.424685] optee: dynamic shared memory is enabled
[ 0.426347] random: crng init done
[ 0.426795] optee: initialized driver
[ 0.427757] NET: Registered PF_PACKET protocol family
[ 0.427783] can: controller area network core
[ 0.427875] NET: Registered PF_CAN protocol family
[ 0.427890] can: raw protocol
[ 0.427904] can: broadcast manager protocol
[ 0.427918] can: netlink gateway - max_hops=1
[ 0.428898] Key type dns_resolver registered
[ 0.429135] ThumbEE CPU extension supported.
[ 0.429162] Registering SWP/SWPB emulation handler
[ 0.485093] registered taskstats version 1
[ 0.485264] Loading compiled-in X.509 certificates
[ 0.539367] scmi_protocol scmi_dev.1: Enabled polling mode TX channel - prot_id:16
[ 0.539678] arm-scmi firmware:scmi: SCMI Notifications - Core Enabled.
[ 0.539806] arm-scmi firmware:scmi: SCMI Protocol v2.0 'ST:' Firmware version 0x0
[ 0.563687] scmi-regulator scmi_dev.5: Regulator reg11 registered for domain [0]
[ 0.584299] scmi-regulator scmi_dev.5: Regulator reg18 registered for domain [1]
[ 0.584820] scmi-regulator scmi_dev.5: Regulator usb33 registered for domain [2]
[ 0.585504] scmi-regulator scmi_dev.5: Regulator vddcpu registered for domain [6]
[ 0.586112] scmi-regulator scmi_dev.5: Regulator vdd registered for domain [8]
[ 0.586728] scmi-regulator scmi_dev.5: Regulator vddcore registered for domain [9]
[ 0.587329] scmi-regulator scmi_dev.5: Regulator vdd_adc registered for domain [10]
[ 0.587730] scmi-regulator scmi_dev.5: Regulator vdd_usb registered for domain [13]
[ 0.588387] scmi-regulator scmi_dev.5: Regulator vdd_sd registered for domain [14]
[ 0.588998] scmi-regulator scmi_dev.5: Regulator v1v8_periph registered for domain [15]
[ 0.589395] scmi-regulator scmi_dev.5: Regulator v3v3_sw registered for domain [19]
[ 0.624740] stm32mp135-pinctrl soc:pinctrl@50002000: GPIOA bank added
[ 0.625493] stm32mp135-pinctrl soc:pinctrl@50002000: GPIOB bank added
[ 0.626228] stm32mp135-pinctrl soc:pinctrl@50002000: GPIOC bank added
[ 0.626984] stm32mp135-pinctrl soc:pinctrl@50002000: GPIOD bank added
[ 0.627718] stm32mp135-pinctrl soc:pinctrl@50002000: GPIOE bank added
[ 0.634572] stm32mp135-pinctrl soc:pinctrl@50002000: GPIOF bank added
[ 0.644703] stm32mp135-pinctrl soc:pinctrl@50002000: GPIOG bank added
[ 0.645539] stm32mp135-pinctrl soc:pinctrl@50002000: GPIOH bank added
[ 0.646355] stm32mp135-pinctrl soc:pinctrl@50002000: GPIOI bank added
[ 0.646398] stm32mp135-pinctrl soc:pinctrl@50002000: Pinctrl STM32 initialized
[ 0.649437] stm32-dma 48000000.dma-controller: STM32 DMA driver registered
[ 0.651637] stm32-dma 48001000.dma-controller: STM32 DMA driver registered
[ 0.675382] stm32-mdma 58000000.dma-controller: STM32 MDMA driver registered
[ 0.684494] stm32-usbphyc 5a006000.usbphyc: registered rev:1.0
[ 0.687172] dwc2 49000000.usb: supply vusb_d not found, using dummy regulator
[ 0.687404] dwc2 49000000.usb: supply vusb_a not found, using dummy regulator
[ 0.824506] dwc2 49000000.usb: EPs: 9, dedicated fifos, 952 entries in SPRAM
[ 0.825499] dwc2 49000000.usb: DWC OTG Controller
[ 0.825552] dwc2 49000000.usb: new USB bus registered, assigned bus number 1
[ 0.825611] dwc2 49000000.usb: irq 41, io mem 0x49000000
[ 0.826908] hub 1-0:1.0: USB hub found
[ 0.827004] hub 1-0:1.0: 1 port detected
[ 0.830549] ehci-platform 5800d000.usb: EHCI Host Controller
[ 0.830604] ehci-platform 5800d000.usb: new USB bus registered, assigned bus number 2
[ 0.831111] ehci-platform 5800d000.usb: irq 42, io mem 0x5800d000
[ 0.836006] stm32_rtc 5c004000.rtc: registered as rtc0
[ 0.836057] stm32_rtc 5c004000.rtc: setting system clock to 2000-01-01T00:00:08 UTC (946684808)
[ 0.836688] stm32_rtc 5c004000.rtc: Date/Time must be initialized
[ 0.836711] stm32_rtc 5c004000.rtc: registered rev:3.3
[ 0.854274] ehci-platform 5800d000.usb: USB 2.0 started, EHCI 1.00
[ 0.855647] hub 2-0:1.0: USB hub found
[ 0.855741] hub 2-0:1.0: 2 ports detected
[ 0.914421] stm32f7-i2c 40012000.i2c: STM32F7 I2C-0 bus adapter
[ 0.954626] stm32f7-i2c 4c006000.i2c: STM32F7 I2C-1 bus adapter
[ 0.974543] stm_thermal 50028000.thermal: stm_thermal_probe: Driver initialized successfully
[ 0.977319] ohci-platform 5800c000.usb: Generic Platform OHCI controller
[ 0.977381] ohci-platform 5800c000.usb: new USB bus registered, assigned bus number 3
[ 0.979047] stm32-usart 40010000.serial: interrupt mode for rx (no dma)
[ 0.979070] stm32-usart 40010000.serial: interrupt mode for tx (no dma)
[ 0.979759] ohci-platform 5800c000.usb: irq 40, io mem 0x5800c000
[ 0.979831] 40010000.serial: ttySTM0 at MMIO 0x40010000 (irq = 49, base_baud = 4000000) is a stm32-usart
[ 0.979896] printk: console [ttySTM0] enabled
[ 2.637742] Freeing initrd memory: 6332K
[ 3.459377] hub 3-0:1.0: USB hub found
[ 3.461797] hub 3-0:1.0: 2 ports detected
[ 3.469934] 4c001000.serial: ttySTM3 at MMIO 0x4c001000 (irq = 50, base_baud = 4000000) is a stm32-usart
[ 3.480613] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 3.487789] clk: Disabling unused clocks
[ 3.493109] Freeing unused kernel image (initmem) memory: 1024K
[ 3.498118] Run /init as init process
Starting systemd-udevd version 255.4^
root '/dev/disk/by-partuuid/491f6117-415d-4f53-88c9-6e0de54deac6' doesn't exist or does not contain a /dev.
[ 33.764208] vddcpu: disabling
[ 33.765818] vdd: disabling
[ 33.768485] vddcore: disabling
[ 33.771565] vdd_sd: disabling
doesn't exist or does not contain a /dev
But when I see the partitions in u-boot everything is ok (userfs 491f6117.... is exists)
STM32MP> mmc list
STM32 SD/MMC: 1 (eMMC)
STM32MP> mmc dev 1
switch to partitions #0, OK
mmc1(part 0) is current device
STM32MP> mmc part
Partition Map for MMC device 1 -- Partition Type: EFI
Part Start LBA End LBA Name
Attributes
Type GUID
Partition GUID
1 0x00000400 0x000007ff "metadata1"
attrs: 0x0000000000000000
type: 8a7a84a0-8387-40f6-ab41-a8b9a5a60d23
(8a7a84a0-8387-40f6-ab41-a8b9a5a60d23)
guid: ed5d1bf6-fed4-4029-a9ac-0e4e6cfcf3ea
2 0x00000800 0x00000bff "metadata2"
attrs: 0x0000000000000000
type: 8a7a84a0-8387-40f6-ab41-a8b9a5a60d23
(8a7a84a0-8387-40f6-ab41-a8b9a5a60d23)
guid: f5cb5b5d-0745-4aa0-92f3-70ed3f914390
3 0x00000c00 0x00002bff "fip-a"
attrs: 0x0000000000000000
type: 19d5df83-11b0-457b-be2c-7559c13142a5
(19d5df83-11b0-457b-be2c-7559c13142a5)
guid: 4fd84c93-54ef-463f-a7ef-ae25ff887087
4 0x00002c00 0x00004bff "fip-b"
attrs: 0x0000000000000000
type: 19d5df83-11b0-457b-be2c-7559c13142a5
(19d5df83-11b0-457b-be2c-7559c13142a5)
guid: 09c54952-d5bf-45af-acee-335303766fb3
5 0x00004c00 0x00004fff "u-boot-env"
attrs: 0x0000000000000000
type: 3de21764-95bd-54bd-a5c3-4abe786f38a8
(u-boot-env)
guid: 71c522d1-5797-48b8-ae67-b6f4abc23c31
6 0x00005000 0x00024fff "bootfs"
attrs: 0x0000000000000004
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: 2b3f174d-1240-43f4-8a87-980af68c4055
7 0x00025000 0x0002cfff "vendorfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: c2237252-2770-47d7-861c-32117b56e405
8 0x0002d000 0x0062cfff "rootfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: 491f6117-415d-4f53-88c9-6e0de54deac6
9 0x0062d000 0x00747bff "userfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
(linux)
guid: 2aa2bce7-16a1-420c-a6e1-e944c8a47e63
STM32MP>
I attached some files (changed name for the attach problem)
Kernel DTS : kernel...dts
u-boot dtsi : uboot-dtsi---xxx.dts
u-boot dts : uboot---xxx.dts
Thank you so much for reading.
Best