Skip to main content
Associate II
Dec 16, 2025 7:28 PM UTC
Solved

STM32MP133C Ethernet/PHY issue

Hello! I'm working on bringing up a bare-metal STM32MP133C bare-metal on the dev kit from DIGI, using the HAL layer from ST. The problem I'm running in to is we're getting stuck on HAL_ETH_Init as when we enable the MAC clock, DMAMR's 0 bit (the reset bit) is stuck at 1, causing a timeout. 

 

From reading the reference manual, all related clocks need to be enabled for the reset to work, so I'm operating under the assumption there's a clock issue. I've initialized/configured the peripheral clock for PLL4, I'm enabling the relevant GPIO clocks, along with the ethernet clocks ETH1CK, ETH1TX, ETH1RX, and ETH1MAC. This leads me to believe the issue may be with the PHY clock. As we're using the Marvell PHY that comes with the board, I've (attempted) to set it so the PHY uses PLL4 by changing the appropriate bits in syscfg's PMCSETR. 

 

I figured that would be enough to get it all going... but it still seems I'm missing something. I've tried generating the code from CubeMX to see if it was a GPIO issue with no luck. I've attached the (very rough) file I'm working out of at present.

 

Thanks in advance for any support provided!

AerokiiBest answer
Associate II
Dec 23, 2025 7:55 PM UTC

Looks like it was a combination of issues. I've been able to get it moving by setting up syscfg, confirming/adding some GPIOs that were not included in either CubeMX or anywhere obvious in the Digi dtsi file, and as recommended, setting PI2. For those who follow in my footsteps, I found this repo helpful as well: GitHub - Oryx-Embedded/CycloneTCP: Dual IPv4/IPv6 Stack.

 

Thanks much for your assistance!

10 replies

Pwxn
ST Employee
Dec 17, 2025 8:20 AM UTC

Hello,

 

Could you give me the version of CubeMX you're using? A similar issue where ETH_DMAMR_SWR stay up during the Init function was fixed with the 6.16 release.

You can applied a Work Around to your current version of CubeMX by replacing __HAL_RCC_ETHxMAC_CLK_ENABLE() (x={1,2}) by __HAL_RCC_ETHxCK_CLK_ENABLE() on line 423 and 505 of stm32mp13xx_hal_msp.c

 

Please use latest version of CubeMX if it's not the case. 

 

Regards

 

AerokiiAuthor
Associate II
Dec 17, 2025 2:55 PM UTC

Of course! It was originally done via 6.15, but I upgraded to 6.16.1 this morning. Sadly it was to no real success, as I'd already added that clock manually.

PatrickF
ST Employee
Dec 17, 2025 5:23 PM UTC

Hi @Aerokii,

 

I also see in your code some GPIO mistakes (still to be confirmed with DIGI documents), for instance:

ETH1_RX_CLK seems to be on PD7-AF10 while you used PA1-AF11

ETH1_CLK125 is not used in your code (should be on PF12-AF11), but you might want to use 125MHz from RCC.


You should check carefully each PHY signals connection usage to STM32MP13 within DIGI HW.

SOM: https://www.digi.com/resources/documentation/digidocs/pdfs/90002551.pdf

BaseBoard: https://hub.digi.com/dp/path=/support/asset/connectcore-mp133-dvk-schematics-pdf/ 

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
AerokiiAuthor
Associate II
Dec 17, 2025 8:16 PM UTC

Hello again!

I've updated the GPIO, at least for ETH1 since that's what I'm focusing on now. It's based on ccmp13-dvk.dtsi along with some confirmations from the provided digi documents. At present I don't have access to a scope, a continuing frustration I've brought up with management, but unrelated to this ticket beyond that. 

Double checking the sent file... I did seem to be using PD7 with AF10, so that shouldn't be an issue. I've double checked it, and I'm attaching the updates. I've still no luck after enabling PF12 in mode AF11, nor with manually setting to 125MHz from the RCC. Still a puzzler, it seems. 

PatrickF
ST Employee
Dec 18, 2025 8:16 AM UTC

Hi,

Did you check the PHY reset pin is released by your SW (sound like it is PI2) ? If you don't have scope, a voltmeter or checking GPIO IDR with debugger might be enough.

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent