Skip to main content
Associate III
Jun 25, 2024 12:34 PM UTC
Solved

STM32MP13 - Jumbo Frames - Constrained MTU size problem

Hi,

 

I am working on an Azure RTOS project, which requires jumbo frames capability. My current devkit is a MYD-YF13X to utilize 1 gigabit ethernet PHYs.

 

My goal is to receive 9000-byte packets, but I am not able to receive any bigger than ~2000 bytes.

Packets with size over 2kB are simply being ignored, as they wouldn't be transferred. The eth interrupts and respective receive complete callbacks are not being activated for them. 

 

I performed the following configuration:

jschneider_0-1719317235312.png

I have also configured the YT8521-SH ethernet PHY to work with jumbo frames

jschneider_1-1719317391252.png

I have also adapted the size of the buffers respectively.

 

At the end I worked with the OpenSTLinux with both STM32MP13-Devkit and MYD-YF13X. I wanted to resize the MTU of eth interface. With the ifconfig tool I wasn't able to set the MTU to 9000 bytes. Once again, it was constrained to 2000 bytes.

jschneider_2-1719318464265.png

Why is the constraint set to ~2000?

 

I would be thankful for any advice and help.

 

Best,

J.Schneider

 

 

This topic has been closed for replies.
jschneiderBest answer
Associate III
Jun 27, 2024 6:43 AM UTC

Hello,

 

I solved the problem.

I just had to reset RSF in ETH_MTLRXQxOMR.

 

Best,

J.Schneider

3 replies

jschneiderAuthorBest answer
Associate III
Jun 27, 2024 6:43 AM UTC

Hello,

 

I solved the problem.

I just had to reset RSF in ETH_MTLRXQxOMR.

 

Best,

J.Schneider

unsigned_char_array
Lead III
Jun 27, 2024 7:49 AM UTC

Can you please share (some of) your code so others know how to do this too?

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
Associate III
Jul 1, 2024 2:29 PM UTC

Hi,

 

Of course, I can share a sample piece of code.

jschneider_0-1719844075798.png

You might also need to consider the assumptions of my first post.

 

Best,

J.Schneider