Skip to main content
ARama.1
Associate II
Jul 13, 2023 6:01 AM UTC
Question

STM32MP1 - VBAT characteristics - need clarity

Hi,

we're using STM32MP1 for our project. we have connected super cap to VBAT.

our expectation is to have VBAT supply power to RTC *alone*. we dont want RAM content to be retained. so that RTC shall remain powered for long time. currently the VBAT is supplying back up power for both RAM contents & also for RTC, so we're experiencing RTC back up for just 5 hours instead of expected 5 days. Kindly help out.

 

should we use RREN/BREN in this case?

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
Jul 21, 2023 12:11 PM UTC

Hi @ARama.1 

To explain the result far below your expectations, I think BREN and RREN are set, so you should change SW (TF-A or opTEE) or DT to remove this setting.

According to datasheet, power with LSE+RTC only should be typically 1.25uA at 3V

Regards.

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent