Skip to main content
debugging
Lead
Jul 5, 2020 5:20 AM UTC
Solved

STM32MP1 UART custom baud rates (Linux)

Apparently it is not possible to set a custom baud rates for UARTs on the STM32MP1.

ioctl TIOCSSERIAL fails. With a USB UART dongle that supports custom baud rates this works. Is there a something that can be changed in the device tree or config to enable custom baud rate support on the STM32MP1 U(S)ARTS ? The base rate seems 4MHz so that should be sufficient for several custom baud rates. Looked at stm32-usart.c but did not find supporting code. Custom baud rate is crucial as the serial device connected must be used with a non standard baud rate.

Edit: after looking at stm32-uart.c it seems it is not supporting ioctl. Adding this support looks to be pretty straightforward by adding the ioctl call and the 2 or 3 needed functions to set and get the user info together with the magic baudrate hack. The driver seems to use uart structure instead of the tty structures so I did not get far changing the driver.. A developer familiar with the driver probably could do this in a day. If STM could reply this post with a beta version of such stm32-uart.c that would be great to be able to move forward.

Edit : Since no reply from ST, have no other option and have started to change the driver myself to add the ioctcl's... and related code.

This topic has been closed for replies.
berendi
berendiBest answer
Principal
Jul 9, 2020 9:15 AM UTC

TIOCSSERIAL looks like deprecated, try TCSETS2

struct termios2 tio;
ioctl(fd, TCGETS2, &tio);
tio.c_cflag &= ~CBAUD;
tio.c_cflag |= BOTHER;
tio.c_ispeed = custom_baudrate;
tio.c_ospeed = custom_baudrate;
ioctl(fd, TCSETS2, &tio);

4 replies

OlivierK
ST Technical Moderator
Jul 8, 2020 8:29 AM UTC

​Hi,

have you already look at this page?

https://wiki.st.com/stm32mpu/wiki/Serial_TTY_overview

you may change the baud rate using this command for instance 4MB/s

/* USART3 port configuration and opening for RX */

cat /proc/tty/driver/stm32-usart                         /* serial counters and modem lines state per UART */

stty -F /dev/ttySTM1 4000000 cs8 -parenb parodd -echo -icanon -onlcr ocrnl onlret crtscts

cat /dev/ttySTM1 &                                          /* port opening for RX, only for tests 2 and 3 */

cat /proc/tty/driver/stm32-usart                         /* serial counters and modem lines state per UART */

0: uart:stm32-usart mmio:0x40010000 irq:52 tx:11212 rx:517 RTS|CTS|DTR|DSR|CD

1: uart:stm32-usart mmio:0x4000F000 irq:50 tx:211 rx:0 CTS|CD

2: uart:stm32-usart mmio:0x40018000 irq:53 tx:0 rx:0 CTS|DSR|CD

Otherwise the serdev interface might be an option.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
debugging
debuggingAuthor
Lead
Jul 9, 2020 7:17 AM UTC

Hi,

Yes I looked at that page, I also checked again and did not find the text you may change the baud rate using this command for instance or /* USART3 port configuration and opening for RX */on that page. Could 4000000 work because this is a high custom baud-rate (actually it is the base rate, so the divider is 1) and not a custom one that is somewhere in the standard defined range, say under 115200 ? my code uses TIOCGSERIAL and TIOCSSERIAL and this works with interfaces/drivers that support custom rates . Looked at the st32-usart.c code and did not found supporting code. I am not sure what stty does to set the rate but will try. I actually wish to set the rate from C code or to the custom rate at boot time. Not familiar with serdev (how to find the ports , how to call the API from C )

berendi
berendiBest answer
Principal
Jul 9, 2020 9:15 AM UTC

TIOCSSERIAL looks like deprecated, try TCSETS2

struct termios2 tio;
ioctl(fd, TCGETS2, &tio);
tio.c_cflag &= ~CBAUD;
tio.c_cflag |= BOTHER;
tio.c_ispeed = custom_baudrate;
tio.c_ospeed = custom_baudrate;
ioctl(fd, TCSETS2, &tio);

debugging
debuggingAuthor
Lead
Jul 12, 2020 12:39 PM UTC

Thanks, that worked.