Skip to main content
Bkell.1
Associate II
Jan 29, 2025 3:33 AM UTC
Question

STM32MP1 I2S on M4 core

Hi, I want to use the M4 core to handle all Audio DSP work

I can see that MXCube allows the SAI ports to be enabled on the M4 core

But it appears the I2S ports are not. 

I am Missing something here

Unfortunately the Pins I need to be  the PZ0-1-2-3 as PCB is done

Bkell1_0-1738121273906.png

Else If Its only possible to use the I2S from the Linux A7 then is it even possible to transfer audio data between the cores?

Thanks

This topic has been closed for replies.