Skip to main content
Michael Schmid
Associate II
May 20, 2019 5:48 AM UTC
Solved

STM32MP fast data exchange between M4 and A7

Dear all,

how can the Cortex-M4 MCU (bare metal or RTOS) exchange data fast with the A7-Linux system? Can the M4 access the DDR RAM of the Linux system, like the PRU on the Beaglebone can do? In the datasheet, there is a connection between the AHB bus and the AXI bus, maked as asynchronous, so it looks like there is a DMA channel for this.

I could not find an example code or project, showing a fast data exchange between the memories of M4 and A7. Does ST provide an example for this?

Thanks,

Michael

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
May 23, 2019 12:35 PM UTC

Hi,

Cortex-M4 is not intended to access DDR content. Cortex-M4 has no cache and asynchronous path to AXI bus has not been optimized for that, so Cortex-M4 performance will be very largely impacted.

Furthermore, accessing small chunk of data to a DDR is never a good choice, as this will affect the DDRCTRL scheduling and so the performance of other AXI masters accessing the DDR SDRAM.

Although it is possible from HW point of view, in our Linux deliveries, Cortex-M4 access is forbidden inside TrustZone address space controller for DDR (TZC).

For data exchange between A7 and M4 please have a look to discussion on this post.

https://community.st.com/s/question/0D50X0000AnuE1XSQU/what-is-the-maximum-transmission-interprocessor-bandwidth-on-stm32mp

Hope it help

BR,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
May 23, 2019 12:35 PM UTC

Hi,

Cortex-M4 is not intended to access DDR content. Cortex-M4 has no cache and asynchronous path to AXI bus has not been optimized for that, so Cortex-M4 performance will be very largely impacted.

Furthermore, accessing small chunk of data to a DDR is never a good choice, as this will affect the DDRCTRL scheduling and so the performance of other AXI masters accessing the DDR SDRAM.

Although it is possible from HW point of view, in our Linux deliveries, Cortex-M4 access is forbidden inside TrustZone address space controller for DDR (TZC).

For data exchange between A7 and M4 please have a look to discussion on this post.

https://community.st.com/s/question/0D50X0000AnuE1XSQU/what-is-the-maximum-transmission-interprocessor-bandwidth-on-stm32mp

Hope it help

BR,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.