Skip to main content
Mario Luzeiro
Associate III
Apr 11, 2022 5:19 PM UTC
Solved

STM32CubeMX assumes GPIO is input while using LL library?

I'm not sure if this is a bug, but STM32CubeMX assumes GPIO is input while using LL library? And is not configuring it to be Input ?

I found that I had to force to configure the pin as Input so it will work with external interrupts.

This topic has been closed for replies.
Aziz BRIGUI
Aziz BRIGUIBest answer
ST Technical Moderator
Apr 13, 2022 1:53 PM UTC

Hello @Mario Luzeiro​  ,

  

You are right, pins should also be configured as inputs when setting up an external interrupt. This is not intended behavior and have been reported.

Internal ticket number: 126386 (This is an internal tracking number and is not accessible or usable by customers).

Thank you for your contribution and sorry for the inconvenience, I will keep you posted with updates on the issue.

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly.

Best regards,

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

5 replies

Nikita91
Lead II
Apr 11, 2022 10:31 PM UTC

I think on most MCUs the default GPIO mode is analog input to lower the power.

LL does not configure GPIO if you do not do it yourself

Aziz BRIGUI
ST Technical Moderator
Apr 12, 2022 12:53 PM UTC

Hello @Mario Luzeiro​ ,

Thank you for your feedback,

Can you provide more explanation to help us reproduce the behavior you observed. For example you can share an IOC file demonstrating the issue, or steps we can follow to get the same results.

Best regards,

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Mario Luzeiro
Associate III
Apr 12, 2022 1:17 PM UTC

ioc attached.

It setups an external interrupt line on rise input, but it does not setup the pin as input.

If I use the same configuration but with HAL library instead of LL, it works (because HAL code initiates it as input, on same function as setting it as external interrupt)

I'm not sure if how the CM4 inits its program, from a "production mode" debug, but it may be that in that case it does not proceed with a proper MCU reset, so the settings may not be as from reset?

Aziz BRIGUI
Aziz BRIGUIBest answer
ST Technical Moderator
Apr 13, 2022 1:53 PM UTC

Hello @Mario Luzeiro​  ,

  

You are right, pins should also be configured as inputs when setting up an external interrupt. This is not intended behavior and have been reported.

Internal ticket number: 126386 (This is an internal tracking number and is not accessible or usable by customers).

Thank you for your contribution and sorry for the inconvenience, I will keep you posted with updates on the issue.

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly.

Best regards,

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Aziz BRIGUI
ST Technical Moderator
Jun 29, 2022 11:22 AM UTC

Hello @Mario Luzeiro​,

Issue fixed in STM32CubeMX latest release.

V6.6.0 is now available under this Link.

Thank you for your contribution.

Best regards,

Aziz.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.