Skip to main content
Lead
Oct 6, 2024 4:21 PM UTC
Question

STM32-OS - An alternative to OpenSTLinux

Hi!

Just want to say that I have made a linux distro called STM32-OS that works with all of STM32MP1.

The reason why I built my own linux distro is because I had a lot of problems with OpenSTLinux and seeing other facing the same issues too. I'm also wanted a rich package system based on Ubuntu 24.04 LTS. Also I did not want to depend on ST's support. There are many reasons.

STM32-OS having support for the same packages as Ubuntu 24.04 LTS have.

  • VNC
  • SSH
  • Qt
  • Mesa
  • etc.

Anyway! Here is the repository to STM32-OS: https://github.com/danielmartensson/STM32-OS

Give it a star. ;) Pullrequest are welcome!

Only run ./create_stm32_os.sh and you will get a file called rootfs.ext4 inside the same folder. Then you can use that .ext4 together with your FlashLayout and flashing your device with STM32CubeProgrammer as usual. The file bootfs.ext4 contains your compiled kernel and .dts file that suits your platform.

This is an example of a FlashLayout that suits STM32-Computer. I have removed the userfs.ext4 and vendorfs.ext4 for saving memory.

 

#Opt	Id	Name	Type	IP	Offset	Binary
-	0x01	fsbl-boot	Binary	none	0x0	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-usb.stm32
-	0x03	fip-boot	FIP	none	0x0	fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
P	0x04	fsbl1	Binary	mmc0	boot1	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P	0x05	fsbl2	Binary	mmc0	boot2	arm-trusted-firmware/tf-a-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.stm32
P	0x06	metadata1	FWU_MDATA	mmc0	0x00080000	arm-trusted-firmware/metadata.bin
P	0x07	metadata2	FWU_MDATA	mmc0	0x00100000	arm-trusted-firmware/metadata.bin
P	0x08	fip-a	FIP	mmc0	0x00180000	fip/fip-stm32mp151a-stm32-computer-firmware-mx-optee-emmc.bin
PED	0x09	fip-b	FIP	mmc0	0x00580000	none
PED	0x0A	u-boot-env	ENV	mmc0	0x00980000	none
P	0x10	bootfs	System	mmc0	0x00A00000	bootfs.ext4
P	0x11	rootfs	FileSystem	mmc0	0x04A00000	rootfs.ext4

 

screen2.jpg 
Yes. Playing Doom works on the STM32MP151 processor.

vnc.jpg

This topic has been closed for replies.