Skip to main content
LLe.1
Associate
Jul 16, 2022 8:39 AM UTC
Question

STM32 board support eDP bridge?

Hi,

We are using stm32mp157c MCU/board and it has DSI output built-in. Now we want to add display port support via DSI to eDP bridge SN65DSI86. It seems that stm32 does not support Displayport output or it has never been done. At least the driver dw_mipi_dsi-stm.c should be updated not to require a panel.

Any idea how this can be achieved please?

This topic has been closed for replies.

34 replies

Erwan SZYMANSKI
ST Technical Moderator
Jul 27, 2022 3:25 PM UTC

Hi @LLe.1​ ,

Do you have any update from your side ? I saw that some patches on the bridge driver also deal with your probe ordering issue, such as this patch.

Maybe it could be interesting to take a look at it.

Regards.

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
LLe.1
LLe.1Author
Associate
Aug 4, 2022 5:04 AM UTC

@Erwan SZYMANSKI​ the patch doesn't help because dw_mipi_dsi_bridge_attach() is called even before ti-bridge probe is called.

I start to think that I will need somehow to get new version of the bridge driver -> new kernel + drm. Or what is your suggestion?

Erwan SZYMANSKI
ST Technical Moderator
Aug 4, 2022 6:58 AM UTC

Hello @LLe.1​,

Sorry to see that the patch is not enough to face your issue.

I think, as you said, that upgrade OSTL version would be a good idea. Your kernel version is quite old now, and if there is no blocker for you to pass on a OSTL 4.0 version, it could be a good idea.

Moreover, as dev team is currently working with this same version, it will be much easier to detect if there are things that go wrong.

Please let me informed about the evolution.

Kind regards.

Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
LLe.1
LLe.1Author
Associate
Aug 7, 2022 9:12 PM UTC

@Erwan SZYMANSKI​ unfortunately upgrading the kernel is not an option for us.

However, I got a bit further, by removing simplepanel's power supply init from panel's probe function, I got panel probe faster and thus solved the probe ordering issue. I don't think panel needs that as it is an external display.

/* commented out
	panel->supply = devm_regulator_get(dev, "power");
	if (IS_ERR(panel->supply))
	{
		DRM_ERROR("PANEL_probe: err supply \n");
		return PTR_ERR(panel->supply);
	}
*/

Now probe and attach order is fine. dsi, bridge are attached. However, after that panel_simple_get_modes() -> panel_simple_get_non_edid_modes() is called and within this function the connector pointer is NULL. Nothing else happens after that, meaning no more action from dsi or bridge.

struct drm_connector *connector = panel->base.connector;
connector is NULL

Any idea please?

LLe.1
LLe.1Author
Associate
Aug 8, 2022 5:17 AM UTC

I am concerning about the location of my simple-panel in device tree, should it be like it is now (under root node), or should it be inside bridge node?

How does simple-panel indicate its presence (when DisplayPort is plugged in) to bridge and dsi so that they start sending data?