Skip to main content
Associate II
Oct 31, 2025 5:45 PM UTC
Question

STM32 ADC UBoot Driver failing when trying to enable ADC voltage regulator (ADVREGEN)

I'm trying to perform ADC using PA3 (adc1_in15) and PF11(adc1_in2) pins of stm32mp157c-ev1 board but I keep getting "stm32-adc adc@0: Failed to enable vreg: -110"

In arch/arm/dts/stm32mp157c-ev1-u-boot.dtsi I added the following:

&adc {
    /* ANA0, ANA1 are dedicated pins and don't need pinctrl: only in6. */
    pinctrl-0 = <&adc1_ain_pins_a>;
    pinctrl-names = "default";
    vdd-supply = <&vdd>;
    vdda-supply = <&vdda>;
    vref-supply = <&vdda>;
    status = "okay";
    adc1: adc@0 {
         status = "okay";
 
        /delete-node/ channel@0;
        /delete-node/ channel@1;
        /delete-node/ channel@6;
 
        channel@2 {
             reg = <2>;
             /* 16.5 ck_cycles sampling time */
            st,min-sample-time-ns = <400>;
        };
        channel@15 {
            reg = <15>;
            st,min-sample-time-ns = <400>;
        };
    };
};
 
After comparing the drivers between the kernel and uboot, I found out that the UBoot's stm32-adc-core driver does not enable the VDDA/VDD and VREF regulators. Thus, I tried to patch 
stm32_adc_core_probe so VDDA/VDD and VREF regulators will get enabled (I used
regulator_set_enable_if_allowed API from regulator.h to enable them)
). After patching it, I verified that the issue got fixed and was able to perform ADC.
 
I would like to understand whether this is a driver issue or DTS issue? If it is a driver problem, please patch it as I'm not an familiar with contributing to the community and got no idea about the SOP for patching a driver. Thanks!
 
This topic has been closed for replies.