Skip to main content
DYenEmbedded
Associate II
Aug 21, 2023 6:32 PM UTC
Question

stLinux kernel version modules path

To workaround path issue with depmod -a 

/lib/modules# cp -r 5.15.67 5.15.67-g8d25ddcc4f56

# /sbin/depmod -a
depmod: ERROR: could not open directory /lib/modules/5.15.67-g8d25ddcc4f56: No such file or directory
depmod: FATAL: could not search modules: No such file or directory

this error is because after compiling some kernel changes, mostly device tree changes, Makefile populates lib/modules/5.15.67 however, how to fix where the modules path is, or what the kernel version is ?

# uname -r
5.15.67-g8d25ddcc4f56

This topic has been closed for replies.

1 reply

Gregory PLANCHON
ST Technical Moderator
Sep 4, 2023 1:46 PM UTC

HI,

You can use the command (echo "" > .scmversion) which allows you to by-pass this auto-generation of kernel version number
Then you'll need to rebuild your kernel, and you should normally be on the same version

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.