Skip to main content
Associate
Aug 11, 2026 7:03 AM UTC
Solved

Standalone Bare-Metal Debug of Cortex-M33 Core via ST-LINK

I am working with an STM32MP257F-EV1 Evaluation Board (board reference MB1936, target device STM32MP257FAI3) and am trying to debug a standalone bare-metal application running on the Cortex-M33 core directly over SWD using ST-Link.

Current Setup

  • Board: STM32MP257F-EV1
  • Board reference: MB1936
  • Target: STM32MP257FAI3
  • Tools: STM32CubeIDE and STM32CubeProgrammer
  • Boot configuration (SW1): Development boot
    • Boot0 = 1
    • Boot1 = 1
    • Boot2 = 0
    • Boot3 = 0
  • JP3: No jumper fitted (STLINK-V3EC active)
  • CubeIDE Debug Configuration:
    • Load Mode = "thru JTAG/SWD link (Engineering mode)"
    • Access Port = "8 - Cortex-M33"
    • Debug interface = SWD

I have also attached a screenshot of the debug error I am receiving.

Current Observation

I am able to debug the Cortex-M33 successfully when the board is first booted from an SD card. After the SD-card boot completes, I can connect to and debug the M33 core from CubeIDE.

However, my requirement is to debug the M33 without booting the board from an SD card, eMMC, or QSPI.

Specifically, I would like to use the STM32MP257F-EV1 as a target for a standalone/bare-metal M33 application, with the debugger connecting directly over SWD and downloading/debugging the application.

Questions

Could you please clarify the following:

  1. Is it possible to debug the Cortex-M33 directly via SWD/JTAG on the STM32MP257F-EV1 without booting from SD card, eMMC, QSPI, or another non-volatile boot source?
  2. What is the recommended and officially supported procedure for debugging a standalone/bare-metal Cortex-M33 application over SWD?​

Any guidance on the required boot process, debug settings, or device configuration would be greatly appreciated.

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Sep 25, 2026 9:39 AM UTC

Hi ​@anilkatta_0977,

No we do not support this M33 standalone debug. 

Due to MP2 HW architecture and RIF related aspect we recommend to stick on “production” mode debug with Linux on A35 side. 

Olivier 

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Sep 25, 2026 9:39 AM UTC

Hi ​@anilkatta_0977,

No we do not support this M33 standalone debug. 

Due to MP2 HW architecture and RIF related aspect we recommend to stick on “production” mode debug with Linux on A35 side. 

Olivier 

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.