Skip to main content
Associate
Feb 21, 2025 11:22 AM UTC
Question

SRAM Usage and Address Ranges on STM32MP25x in OpenSTLinux

I'm using the Yocto-based OpenSTLinux embedded software on a STM32MP25x and I don't understand which portion of the SRAM1/2 is free to use at runtime.

drodr_0-1740134540566.png

Aside from the first 4kBytes of the SRAM1 reserved for OTP shadow, can the rest be fully used, or is it also reserved ?

Additionally, in chapter 2.4.2 of the reference manual (RM0457), it states that SRAM1/2 can be accessed through the following address ranges [0x0A04 0000, 0x0A08 0000[, [0x0E04 0000, 0x0E08 0000[, [0x2004 0000, 0x2008 0000[ and [0x3004 0000, 0x3008 0000[. Why are there four physical addresses for SRAM ? Should Cortex-A35 and Cortex-M33 use specific regions to communicate with each other ?

 

 

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
Feb 21, 2025 5:22 PM UTC

Hi @drodr 

regarding the 4 possible address ranges to access same memories, this is due to the Cortex-M33 address space split between Code and SRAM and secure/non-secure split done with IDAU.
This allows full flexibility for your secure/non-secure code+data applications in a single set of contiguous memories (need to play with different load and execution address in linker).


See PM0264 and RM0457

PatrickF_0-1740158230074.png

PatrickF_1-1740158260480.png

 

Regards

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
drodrAuthor
Associate
Mar 3, 2025 8:10 AM UTC

Hi @PatrickF


Thank you for your answer !

I don't understand how applications are detected "secure/non-secure". Is there something specific that needs to be done to make them run in one mode or the other?

What do you mean by "need to play with different load and execution address in linker" ?

 

Regards