Skip to main content
Grodriguez
Associate III
Jan 30, 2020 5:43 PM UTC
Question

Slow link up times with Gigabit Ethernet on the STM32MP1

I am testing Ethernet on the STM32MP1 (on both the EV1 and DK2 eval boards) and seeing slow link up times when the board is connected to a Gigabit Ethernet switch. Here's an excerpt from the dmesg traces showing link up times of 6-7 seconds:

[ 8.931934] Generic PHY stmmac-0:00: attached PHY driver [Generic PHY] (mii_bus:phy_addr=stmmac-0:00, irq=POLL)
[ 8.952777] dwmac4: Master AXI performs any burst length
[ 8.956664] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 8.964160] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 8.972895] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 14.169871] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx

Since my application does not really need Gigabit Ethernet, I tried limiting the speed to 100 Mbps in the device tree, as described here: https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration

However the results are still similar; typical link up times are in the ~6 second range.

Is there any way to shorten the link up times?

BR,

Guillermo

This topic has been closed for replies.

4 replies

Olivier GALLIEN
ST Technical Moderator
Feb 21, 2020 2:48 PM UTC

Hi @Grodriguez​ 

did you try to use static address to remove DHCP request ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Grodriguez
Associate III
Feb 24, 2020 10:07 AM UTC

Hi Olivier,

Yes, I tested with static address, anyway note that the issue is related to the link time (Ethernet level), not to the IP configuration.

Guillermo

Macdog
Associate III
Jul 17, 2020 7:47 PM UTC

I am also testing the stm32mp157c-dk2 eval board with a buildroot generated, and am also seeing the exact same Ethernet link-up delay, also in the ~6 second range. Is there any way to improve the link-up timing?

Macdog
Associate III
Jul 17, 2020 7:48 PM UTC

Sorry I am new to the forum, didn't mean to attach the log, wanted to display:

Starting network: [  3.327679] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [RTL8211F Gigabit Ethernet]

[  3.368439] dwmac4: Master AXI performs any burst length

[  3.375121] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found

[  3.386583] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported

[  3.399417] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock

[  3.409993] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode

[  9.067672] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx

[  9.080502] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready