Skip to main content
This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
Jul 18, 2025 12:26 PM UTC

Hi @OskarM ,

 

Sorry can you please add further contex and detail about your question ? 

Thanks

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
OskarMAuthor
Associate III
Jul 22, 2025 5:08 PM UTC

Olivier,

the general context is that we almost used out all GPIOs and we have a conflict between M4 and A7 cores on one EXTI "signal". In cores like M4 and any other, simpler cores, when both GPIOs are on the same core, you could just read the current state of both GPIO lines in the interrupt routine and decide which GPIO triggered the acutal EXTI interrupt, provided that we have some knowledge (control) on the external trigger duration etc. It's not perfect, but it's possible to do. Now, when the same situation happens on two, separate cores, each core would have to be triggered on the same EXTI interrupt, maybe use HSEM to protect EXTI registers from clearing the INT flag or...? Quite complicated I guess. 

b.r.