Skip to main content
Associate II
Aug 1, 2025 1:01 PM UTC
Question

Sending Data from M4 to A7 using OpenAMP without A7 Initiation – Need Help!

Greetings everyone,

I’m currently working on inter-core communication between the Cortex-M4 and Cortex-A7 cores using OpenAMP and RPMsg. My goal is to send dummy sensor data from the M4 to the A7 periodically. I am using STM32MP157F-DK2.

However, I’ve noticed an issue:

  • The data from the M4 only gets flushed to the A7 after the A7 writes something first on the virtual channel.

  • In other words, the M4 seems to need some kind of trigger from the A7 before its messages are actually delivered.

What I want to achieve is:
Send data from the M4 to the A7 automatically, without any prior message or intimation from the A7.

Has anyone faced a similar situation or knows how to configure OpenAMP/RPMsg so the M4 can push data independently? Any guidance or code example would be highly appreciated.

I am attaching my main.c below.

int main(void)
{



 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */
 srand(HAL_GetTick());

 MX_IPCC_Init();
 /* OpenAmp initialisation ---------------------------------*/
 MX_OPENAMP_Init(RPMSG_REMOTE, NULL);
 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 /* USER CODE BEGIN 2 */
	/* ##-1- Create Virtual UART device
	 * defined by a rpmsg channel attached to the remote device
	 */
	huart0.rvdev = &rvdev;
	print_string("Virtual UART0 OpenAMP-rpmsg channel creation\r\n");
	if (VIRT_UART_Init(&huart0) != VIRT_UART_OK) {
		print_string("VIRT_UART_Init UART0 failed.\r\n");
		while (1) {
		}
	}


	huart1.rvdev = &rvdev;
	print_string("Virtual UART1 OpenAMP-rpmsg channel creation\r\n");
	if (VIRT_UART_Init(&huart1) != VIRT_UART_OK) {
		print_string("VIRT_UART_Init UART1 failed.\r\n");
		while (1) {
		}
	}
	/*Need to register callback for message reception by channels*/
	if (VIRT_UART_RegisterCallback(&huart0, VIRT_UART_RXCPLT_CB_ID,
			VIRT_UART0_RxCpltCallback) != VIRT_UART_OK) {
		while (1) {
		}
	}
	if (VIRT_UART_RegisterCallback(&huart1, VIRT_UART_RXCPLT_CB_ID,
			VIRT_UART1_RxCpltCallback) != VIRT_UART_OK) {
		while (1) {
		}
	}

 while (1) {
 OPENAMP_check_for_message(); // Handle any messages from A7

 // Generate dummy GPS and IMU values
 float latitude = 12.9000f + ((float)(rand() % 1000) / 10000.0f);
 float longitude = 77.6000f + ((float)(rand() % 1000) / 10000.0f);
 float imu_angle = (float)(rand() % 360);

 char msg[128];

 // Send GPS
 snprintf(msg, sizeof(msg), "GPS:%.5f,%.5f\r\n", latitude, longitude);
 print_string(msg);
 HAL_GPIO_TogglePin(GPIOH, GPIO_PIN_7);

 // Send IMU
 snprintf(msg, sizeof(msg), "IMU:%.2f\r\n", imu_angle);
 print_string(msg);
 HAL_GPIO_TogglePin(GPIOH, GPIO_PIN_7);

 HAL_Delay(500); // 1Hz update rate
 }


	 /* USER CODE END 3 */
 }

void print_string(const char *s)
{
 int l;
 l = strlen(s);
	VIRT_UART_Transmit(&huart0, (uint8_t*) s, l);
}

void VIRT_UART0_RxCpltCallback(VIRT_UART_HandleTypeDef *huart)
{

 	print_string("Msg received on VIRTUAL UART0 channel \n\r");

 /* copy received msg in a variable to sent it back to master processor in main infinite loop*/
 VirtUart0ChannelRxSize = huart->RxXferSize < 100? huart->RxXferSize : 99;
 memcpy(VirtUart0ChannelBuffRx, huart->pRxBuffPtr, VirtUart0ChannelRxSize);
 VirtUart0RxMsg = SET;
}

void VIRT_UART1_RxCpltCallback(VIRT_UART_HandleTypeDef *huart)
{

	print_string("Msg received on VIRTUAL UART1 channel \n\r");
 /* copy received msg in a variable to sent it back to master processor in main infinite loop*/
 VirtUart1ChannelRxSize = huart->RxXferSize < 100? huart->RxXferSize : 99;
 memcpy(VirtUart1ChannelBuffRx, huart->pRxBuffPtr, VirtUart1ChannelRxSize);
 VirtUart1RxMsg = SET;
}

Thank you in advance!

This topic has been closed for replies.

1 reply

Erwan SZYMANSKI
ST Technical Moderator
Aug 7, 2025 1:54 PM UTC

Hello @VedantK33 ,
Unfortunately this is a constraint on MP15 that we must deal with. Most of time, just sending an init message from A7 after the M4 launch is not a huge issue, but I can understand it can not perfectly fit with the implementation you want to do. We have not solution for this today as far as I know.

Thanks for your interest.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.