Skip to main content
Kvan .21
Associate II
February 23, 2026
Question

SD-Card Read Issue

  • February 23, 2026
  • 5 replies
  • 471 views

Hi Community,

We are encountering an issue with the SD-Card on our STM32MP15x board. The problem is, that writing to the SD card works well but the reading does show sporadic errors.

In our configuration, we use 1TB MicroSD-Cards in the DDR50 Mode. In DDR25 mode, the SD card is working fine. Unfortunately, we need the DDR50 Mode (or faster) for our product.

First, let me describe the test scenario: I wrote ~500GB uint64_t ramp data in little endian byte order to a SD-Card, and verified on an external device, that the ramp data have been written correctly. A dump of the first 64 bytes looks as follows:

root@gdl1-31:~# hexdump -C -n 64 /dev/mmcblk0
00000000 00 00 00 00 00 00 00 00 01 00 00 00 00 00 00 00 |................|
00000010 02 00 00 00 00 00 00 00 03 00 00 00 00 00 00 00 |................|
00000020 04 00 00 00 00 00 00 00 05 00 00 00 00 00 00 00 |................|
00000030 06 00 00 00 00 00 00 00 07 00 00 00 00 00 00 00 |................|
00000040


In the next step, I wrote a little test program in C validating the ramp data on our STM32MP15x board. The program outputs random validation errors where the read ramp value differs from the expected one. I could identify, that these errors occur in blocks of 1044480 bytes (1020 KiB). After that block, the read ramp values match the expected ones again (The expected value is a monotonic counter incremented for each read uint64_t value even during validation errors).

Here is an example excerpt of the validation output (the values are dumped in big endian for better readability):

[...]
Progress 2.1% (10.2 GB / 480.0 GB)
Progress 2.2% (10.8 GB / 480.0 GB)
[read address] [expected value] [read value] <--- columns
000000009218FFB8 [exp] 00 00 00 00 52 43 1F F7 [read] 00 00 00 00 52 43 1F F7
000000009218FFC0 [exp] 00 00 00 00 52 43 1F F8 [read] 00 00 00 00 52 43 1F F8
000000009218FFC8 [exp] 00 00 00 00 52 43 1F F9 [read] 00 00 00 00 52 43 1F F9
000000009218FFD0 [exp] 00 00 00 00 52 43 1F FA [read] 00 00 00 00 52 43 1F FA
000000009218FFD8 [exp] 00 00 00 00 52 43 1F FB [read] 00 00 00 00 52 43 1F FB
000000009218FFE0 [exp] 00 00 00 00 52 43 1F FC [read] 00 00 00 00 52 43 1F FC
000000009218FFE8 [exp] 00 00 00 00 52 43 1F FD [read] 00 00 00 00 52 43 1F FD
000000009218FFF0 [exp] 00 00 00 00 52 43 1F FE [read] 00 00 00 00 52 43 1F FE
000000009218FFF8 [exp] 00 00 00 00 52 43 1F FF [read] 00 00 00 00 52 43 1F FF
[Start of error section at byte address: 0x292190000]
0000000092190000 [exp] 00 00 00 00 52 43 20 00 [read] 20 30 05 94 02 00 00 00
0000000092190008 [exp] 00 00 00 00 52 43 20 01 [read] 20 30 05 A4 02 00 00 00
0000000092190010 [exp] 00 00 00 00 52 43 20 02 [read] 20 30 05 B4 02 00 00 00
0000000092190018 [exp] 00 00 00 00 52 43 20 03 [read] 20 30 05 C4 02 00 00 00
0000000092190020 [exp] 00 00 00 00 52 43 20 04 [read] 20 30 05 D4 02 00 00 00
0000000092190028 [exp] 00 00 00 00 52 43 20 05 [read] 20 30 05 E4 02 00 00 00
0000000092190030 [exp] 00 00 00 00 52 43 20 06 [read] 20 30 05 F4 02 00 00 00
0000000092190038 [exp] 00 00 00 00 52 43 20 07 [read] 20 30 05 04 02 01 00 00
0000000092190040 [exp] 00 00 00 00 52 43 20 08 [read] 20 30 05 14 02 01 00 00
0000000092190048 [exp] 00 00 00 00 52 43 20 09 [read] 20 30 05 24 02 01 00 00
0000000092190050 [exp] 00 00 00 00 52 43 20 0A [read] 20 30 05 34 02 01 00 00
0000000092190058 [exp] 00 00 00 00 52 43 20 0B [read] 20 30 05 44 02 01 00 00
0000000092190060 [exp] 00 00 00 00 52 43 20 0C [read] 20 30 05 54 02 01 00 00
0000000092190068 [exp] 00 00 00 00 52 43 20 0D [read] 20 30 05 64 02 01 00 00
0000000092190070 [exp] 00 00 00 00 52 43 20 0E [read] 20 30 05 74 02 01 00 00
0000000092190078 [exp] 00 00 00 00 52 43 20 0F [read] 20 30 05 84 02 01 00 00
0000000092190080 [exp] 00 00 00 00 52 43 20 10 [read] 20 30 05 94 02 01 00 00
-------------------------------------------------
(Skipping further messages for this error section
-------------------------------------------------
000000009228EFB8 [exp] 00 00 00 00 52 45 1D F7 [read] 00 00 00 00 4F F5 EF F7
000000009228EFC0 [exp] 00 00 00 00 52 45 1D F8 [read] 00 00 00 00 4F F5 EF F8
000000009228EFC8 [exp] 00 00 00 00 52 45 1D F9 [read] 00 00 00 00 4F F5 EF F9
000000009228EFD0 [exp] 00 00 00 00 52 45 1D FA [read] 00 00 00 00 4F F5 EF FA
000000009228EFD8 [exp] 00 00 00 00 52 45 1D FB [read] 00 00 00 00 4F F5 EF FB
000000009228EFE0 [exp] 00 00 00 00 52 45 1D FC [read] 00 00 00 00 4F F5 EF FC
000000009228EFE8 [exp] 00 00 00 00 52 45 1D FD [read] 00 00 00 00 4F F5 EF FD
000000009228EFF0 [exp] 00 00 00 00 52 45 1D FE [read] 00 00 00 00 4F F5 EF FE
000000009228EFF8 [exp] 00 00 00 00 52 45 1D FF [read] 00 00 00 00 4F F5 EF FF
[End of error section at byte address: 0x29228F000]
000000009228F000 [exp] 00 00 00 00 52 45 1E 00 [read] 00 00 00 00 52 45 1E 00
[Completed error section of 1044480 Bytes (1020KiB)]
Number of error sections so far: 8

Progress 1.3% (6.1 GB / 480.0 GB)
Progress 1.4% (6.7 GB / 480.0 GB)
Progress 1.5% (7.2 GB / 480.0 GB)

[...]


The incorrect data also seem to be ramp data, but from another region of the Card. Additionally, they are not uint64_t aligned: they seem to be shifted by a number of nibbles (4-bit). This can be seen in the example, because the counting digit is the upper nibble of a byte.

Other error blocks show only a small shift regarding the expected data, like in this example:

000000006B1EBFE0 [exp] 00 00 00 00 8D 63 D7 FC [read] 00 00 00 00 8D 63 D7 FC
000000006B1EBFE8 [exp] 00 00 00 00 8D 63 D7 FD [read] 00 00 00 00 8D 63 D7 FD
000000006B1EBFF0 [exp] 00 00 00 00 8D 63 D7 FE [read] 00 00 00 00 8D 63 D7 FE
000000006B1EBFF8 [exp] 00 00 00 00 8D 63 D7 FF [read] 00 00 00 00 8D 63 D7 FF
[Start of error section at byte address: 0x46B1EC000]
000000006B1EC000 [exp] 00 00 00 00 8D 63 D8 00 [read] D8 01 00 00 00 00 8D 63
000000006B1EC008 [exp] 00 00 00 00 8D 63 D8 01 [read] D8 02 00 00 00 00 8D 63
000000006B1EC010 [exp] 00 00 00 00 8D 63 D8 02 [read] D8 03 00 00 00 00 8D 63
000000006B1EC018 [exp] 00 00 00 00 8D 63 D8 03 [read] D8 04 00 00 00 00 8D 63
000000006B1EC020 [exp] 00 00 00 00 8D 63 D8 04 [read] D8 05 00 00 00 00 8D 63
000000006B1EC028 [exp] 00 00 00 00 8D 63 D8 05 [read] D8 06 00 00 00 00 8D 63

 

 Other observations:

  • The error blocks always start at 12-bit aligned addresses (the lower 3 nibbles of the address are 0).
  • The error blocks seem to occur at random addresses. When starting another validation run, the errors are at different addresses compared to the previous run.
  • The frequency of the errors also seems random, sometimes 10-20 GB can be read without validation error.
  • The Kernel log does not show any I/O errors or other storage related issues.

Any ideas what could go wrong? Any idea is welcome to be tested... Thanks in advance!

Best regards,
Karsten

5 replies

PatrickF
ST Employee
February 23, 2026

Hi @Kvan .21 

Are the IOs speed correctly set ? I

Could you share your HW around level translator (as SDR25 and DDR50 are UHS-I, so 1.8V IOs with 3V supply) ? what is your VDD voltage ?

Is your level translator IC able to do 50MHz with enough timing margins ? Did you check waveforms ? On ICs with auto-direction there might be some issues which might need lower pull-up values on STM32MP15 side.

Did you follow AN5031 recommendations overall?

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Kvan .21
Kvan .21Author
Associate II
February 24, 2026

Hi Patrick,

thank you for your fast response :smiling_face_with_smiling_eyes:.

Our pins are configured as follows:

sdcard pin config.png

The medium speed setting for the data lines is the default value for CuebMX, but we tested already with higher speeds without success.

Regarding our Hardware:

We are using the NXP NVT4858 (https://www.nxp.com/docs/en/data-sheet/NVT4857UK.pdf) auto direction level shifter which is capable of up to 208MHz. The IO Voltage of the MPU is 1V8 and we are using the recommendations from your AN, we have added some 22R resistor in series to reduce ringing. At the beginning we start up the card at 3.3V and we switch to 1V8 IO Voltage for the datalanes during the mode transition. One difference is that we do not use a dedicated pull-down at the CLK_IN path.

Schematic: 

Kvan21_0-1771926983161.jpeg

Can you elaborate the problems with auto dir level shifters and what are the recommendations for the corresponding pull-ups?

Best regards,

Karsten

PatrickF
ST Employee
February 24, 2026

Hi,

as there is only one VDD rail on STM32MP15, I assume you have whole GPIOs at 1.8V.
Did you manage to set both the OTP (PRODUCT_BELOW_2V5) and HSLVEN_SDMMC ?

Worth to look at signals and timings to double check potential issues wrt STM32MP15 SDMMC timings and SD-Card timings (need to probe signals on both sides of the level translators).

Beware of using "very high speed" config as this could lead to overshoot/undershoot (i.e. ringing glitches). Recommendation for DDR50 is "medium speed" for all SDMMC signals.

Did you use the right DTS controls for CKIN usage ?

https://wiki.st.com/stm32mpu/wiki/SDMMC_device_tree_configuration#DT_configuration_-28board_level-29

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Kvan .21
Kvan .21Author
Associate II
March 6, 2026

Hi Patrick,

we double-checked everything you mentioned on our side, but unfortunately could not fix the problem.

Can you elaborate the problems with auto dir level shifters and what are the recommendations for the corresponding pull-ups? We are not totally sure here with our setup.

Is it possible that the error lies in MP1, e.g., DMA handling? It's very noticeable that the length of an erroneously read block is always exactly the same. Or do you have another explanation that could produce precisely this error pattern?

We are grateful for any help. Thanks in advance.

Best regards,

Karsten