Skip to main content
jasonj2
Associate III
Jun 3, 2024 12:47 PM UTC
Solved

SAI2 MCLK not set, codec cannot get MCLK freq

Hello everyone, 

I am trying to debug a custom board with STM32MP151 with WM8988 connected with SAI2, the connection is just as  STM32MP15x-DK with except that there is no I2S to HDMI. The device tree configuration is a mimic of STM32MP15xx-dkx.dtsi. After bootup, the soundcard was created, and I can run alsamixer.

The problem is whenever I try to play a sound, the driver complains about cannot get MCLK because the freq passed to wm8988_set_dai_sysclk() is zero. The log messages shown that the asoc try to configure the dai, but it passed the wrong MCLK freq to wm8988 dai. I don't know why? Is there something I am missing in the device tree? 

Also, I tried to enable DEBUG in stm32_sai_sub.c and find that stm32_sai_mclk_enable() may not be called because I cannot find “Enable master clock” in dmesg.

 

I am using openstlinux eco system 4, the distro version is 4.0.11.

 

Here is the snipet of the device tree. 

&i2c4{
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&i2c4_pins_z_mx>;
	pinctrl-1 = <&i2c4_sleep_pins_z_mx>;
	status = "okay";

	/* USER CODE BEGIN i2c4 */
	i2c-scl-rising-time-ns = <185>;
	i2c-scl-falling-time-ns = <20>;
	clock-frequency = <100000>;

	wm8988: wm8988@1b {
		compatible = "wlf,wm8988";
		#sound-dai-cells = <0>;
		reg = <0x1b>;
		status = "okay";

		DBVDD-supply = <&v3v3>;
		DCVDD-supply = <&v3v3>;
		AVDD-supply = <&vcc_audio>;
		HPVDD-supply = <&vcc_audio>;
	
		clocks = <&sai2a>;
		clock-names = "MCLK";

		ports {
			#address-cells = <1>;
			#size-cells = <0>;

			wm8988_tx_endpoint: port@0 {
				reg = <0>;
				remote-endpoint = <&sai2a_endpoint>;
				frame-master;// = <&wm8988_tx_endpoint>;
				bitclock-master;// = <&wm8988_tx_endpoint>;
			};

			wm8988_rx_endpoint: port@1 {
				reg = <1>;
				remote-endpoint = <&sai2b_endpoint>;
				frame-master;// = <&wm8988_rx_endpoint>;
				bitclock-master;// = <&wm8988_rx_endpoint>;
			};
		};
	};

	/* USER CODE END i2c4 */
};

&sai2{
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&sai2a_pins_mx>, <&sai2b_pins_mx>;
	pinctrl-1 = <&sai2a_sleep_pins_mx>, <&sai2b_sleep_pins_mx>;
	status = "okay";

	/* USER CODE BEGIN sai2 */
	clocks = <&rcc SAI2>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
	clock-names = "pclk", "x8k", "x11k";
	/* USER CODE END sai2 */

	sai2a: audio-controller@4400b004{
		status = "okay";

		/* USER CODE BEGIN sai2a */
		#clock-cells = <0>;
		dma-names = "tx";

		 sai2a_port: port {
			sai2a_endpoint: endpoint {
				remote-endpoint = <&wm8988_tx_endpoint>;
				format = "i2s";
				mclk-fs = <256>;
				dai-tdm-slot-num = <2>;
				dai-tdm-slot-width = <32>;
			};
		};
		/* USER CODE END sai2a */
	};

	sai2b: audio-controller@4400b024{
		status = "okay";

		/* USER CODE BEGIN sai2b */
		dma-names = "rx";
		st,sync = <&sai2a 2>;
		clocks = <&rcc SAI2_K>, <&sai2a>;
		clock-names = "sai_ck", "MCLK";

		sai2b_port: port {
			sai2b_endpoint: endpoint {
				remote-endpoint = <&wm8988_rx_endpoint>;
				format = "i2s";
				mclk-fs = <256>;
				dai-tdm-slot-num = <2>;
				dai-tdm-slot-width = <32>;
			};
		};
		/* USER CODE END sai2b */
	};
};

/ {	
	sound: sound {
		compatible = "audio-graph-card";
		// label = "BM32MP15-Audio-Card";
		label = "STM32MP15DK";

		widgets = 
			"Headphone", "Headphone Jack",
			"Microphone", "Microphone Jack",
			"Speaker", "Speaker External";
		
		routing =
			"Speaker External", "LOUT2",
			"Speaker External", "ROUT2",
			"Headphone Jack", "ROUT1",
			"Headphone Jack", "LOUT1",
			"Playback", "MCLK",
			"Capture", "MCLK";

		dais = <&sai2a_port &sai2b_port>;
		status = "okay";
	};
};

 

Here is the dmesg logs related to sai,  codec, and card. The last six lines were outputed after I try to play a sound by 'speaker-test -t sine‘.

[ 35.334229] platform 4400b004.audio-controller: Fixing up cyclic dependency with 1-001b
[ 35.397741] spi_stm32 4000b000.spi: driver initialized (master mode)
[ 35.453774] platform 4400b024.audio-controller: Fixing up cyclic dependency with 1-001b
[ 35.588275] wm8988 1-001b: wm8988_i2c_probe
[ 35.591486] wm8988: probe of 1-001b failed with error 517
[ 35.651872] wm8988 1-001b: wm8988_i2c_probe
[ 35.655040] wm8988: probe of 1-001b failed with error 517
[ 37.854538] using random self ethernet address
[ 37.905182] using random host ethernet address
[ 38.125237] usb0: HOST MAC 04:5e:be:d5:a7:58
[ 38.148229] usb0: MAC da:21:72:16:95:ef
[ 38.158513] dwc2 49000000.usb-otg: bound driver configfs-gadget
[ 38.871318] wm8988 1-001b: wm8988_i2c_probe
[ 38.874543] wm8988: probe of 1-001b failed with error 517
[ 38.883777] st,stm32-sai-sub 4400b004.audio-controller: Register master clock sai2a_mclk
[ 38.919012] st,stm32-sai-sub 4400b024.audio-controller: 4400b024.audio-controller synchronized with audio-controller@4400b004
[ 38.919087] st,stm32-sai-sub 4400b024.audio-controller: sai->sai_mclk = -1001602112
[ 38.947195] wm8988 1-001b: wm8988_i2c_probe
[ 38.983375] wm8988 1-001b: wm8988->mclk_handle = c44cc700
[ 39.051048] st,stm32-sai-sub 4400b004.audio-controller: Masks tx/rx:0x3/0x3, slots:2, width:32
[ 39.051530] st,stm32-sai-sub 4400b004.audio-controller: fmt 1001
[ 39.052755] st,stm32-sai-sub 4400b024.audio-controller: Masks tx/rx:0x3/0x3, slots:2, width:32
[ 39.063902] st,stm32-sai-sub 4400b024.audio-controller: fmt 1001
[ 39.063952] st,stm32-sai-sub 4400b024.audio-controller: Synchronized SAI configured as slave
[ 39.589379] RESIZE-HELPER START
[ 40.099033] RESIZE-HELPER: Using systemd-growfs
[ 40.156450] EXT4-fs (mmcblk0p10): resizing filesystem from 753664 to 753664 blocks
[ 40.222898] EXT4-fs (mmcblk0p8): resizing filesystem from 65536 to 65536 blocks
[ 40.282788] EXT4-fs (mmcblk0p9): resizing filesystem from 16384 to 16384 blocks
[ 40.342421] EXT4-fs (mmcblk0p11): resizing filesystem from 727516 to 727518 blocks
[ 40.358282] EXT4-fs (mmcblk0p11): resized filesystem to 727518
[ 40.410548] Filesystem Size Used Avail Use% Mounted on
 devtmpfs 178M 0 178M 0% /dev
 /dev/mmcblk0p10 685M 125M 525M 20% /
 tmpfs 245M 0 245M 0% /dev/shm
 tmpfs 98M 8.6M 90M 9% /run
 tmpfs 4.0M 0 4.0M 0% /sys/fs/cgroup
 tmpfs 245M 0 245M 0% /tmp
 /dev/mmcblk0p8 55M 13M 39M 25% /boot
 /dev/mmcblk0p9 14M 6.0M 6.7M 48% /vendor
 /dev/mmcblk0p11 660M 148K 620M 1% /usr/local
 tmpfs 245M 0 245M 0% /var/volatile
[ 40.488909] RESIZE-HELPER FINISH
[ 40.906720] RESIZE-HELPER START
[ 41.013085] RESIZE-HELPER: Using systemd-growfs
[ 41.058996] EXT4-fs (mmcblk0p10): resizing filesystem from 753664 to 753664 blocks
[ 41.090163] EXT4-fs (mmcblk0p8): resizing filesystem from 65536 to 65536 blocks
[ 41.121164] EXT4-fs (mmcblk0p9): resizing filesystem from 16384 to 16384 blocks
[ 41.152169] EXT4-fs (mmcblk0p11): resizing filesystem from 727518 to 727518 blocks
[ 41.173337] Filesystem Size Used Avail Use% Mounted on
 devtmpfs 178M 0 178M 0% /dev
 /dev/mmcblk0p10 685M 125M 525M 20% /
 tmpfs 245M 0 245M 0% /dev/shm
 tmpfs 98M 8.6M 90M 9% /run
 tmpfs 4.0M 0 4.0M 0% /sys/fs/cgroup
 tmpfs 245M 0 245M 0% /tmp
 /dev/mmcblk0p8 55M 13M 39M 25% /boot
 /dev/mmcblk0p9 14M 6.0M 6.7M 48% /vendor
 /dev/mmcblk0p11 660M 148K 620M 1% /usr/local
 tmpfs 245M 0 245M 0% /var/volatile
[ 41.234053] RESIZE-HELPER FINISH
[ 44.718102] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 44.768910] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 45.237727] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:01] driver [RTL8211F Gigabit Ethernet] (irq=POLL)
[ 45.258267] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 45.275609] dwmac4: Master AXI performs any burst length
[ 45.287727] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 45.293887] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 45.334072] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 45.350189] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 48.570866] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 48.587664] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 280.586461] wm8988 1-001b: No MCLK configured, call set_sysclk() on init
[ 280.591971] wm8988 1-001b: ASoC: error at snd_soc_dai_startup on wm8988-hifi: -22
[ 280.605747] wm8988 1-001b: set sysclk, freq = 0
[ 280.612190] wm8988 1-001b: could not set sysclk, freq = 0
[ 280.616181] wm8988 1-001b: ASoC: error at snd_soc_dai_set_sysclk on wm8988-hifi: -22
[ 280.627751] 4400b004.audio-controller-wm8988-hifi: __soc_pcm_open() failed (-22)

 

Here is the lsmod output:

Module Size Used by
cfg80211 651264 0
stm32_adc 36864 0
stm32_timer_trigger 20480 1 stm32_adc
stm32_lptimer_trigger 16384 1 stm32_adc
snd_soc_stm32_sai_sub 28672 8
pwm_stm32 20480 0
snd_soc_audio_graph_card 16384 0
snd_soc_simple_card_utils 20480 1 snd_soc_audio_graph_card
stm32_adc_core 20480 0
stm32_timers 16384 1 pwm_stm32
snd_soc_stm32_sai 16384 0
spi_stm32 24576 0
usb_f_ncm 24576 2
u_ether 20480 1 usb_f_ncm
libcomposite 49152 10 usb_f_ncm
sch_fq_codel 20480 3
snd_soc_wm8988 28672 1
snd_soc_core 180224 4 snd_soc_audio_graph_card,snd_soc_wm8988,snd_soc_simple_card_utils,snd_soc_stm32_sai_sub
snd_pcm_dmaengine 16384 1 snd_soc_core
snd_pcm 94208 4 snd_pcm_dmaengine,snd_soc_wm8988,snd_soc_core,snd_soc_stm32_sai_sub
snd_timer 28672 1 snd_pcm
snd 53248 4 snd_timer,snd_soc_core,snd_pcm,snd_soc_stm32_sai_sub
soundcore 16384 1 snd
fusb302 28672 0
tcpm 65536 1 fusb302
typec 36864 1 tcpm
ip_tables 24576 0
x_tables 24576 1 ip_tables
ipv6 507904 28

 

Here is the output of clk_summary:

 pll3 1 1 0 417755859 0 0 50000 Y
 pll3_r 0 0 0 11290699 0 0 50000 N
 pll3_q 0 0 0 24573875 0 0 47058 N
 sai2_k 0 0 0 24573875 0 0 50000 N
 sai2a_mclk 0 0 0 0 0 0 50000 ?

 

Here is the output of 'ls /dev/snd'

by-path controlC0 pcmC0D0p pcmC0D1c timer

 

Thanks and any comments would be appreciated.

This topic has been closed for replies.
Christophe Guibout
ST Technical Moderator
Jun 6, 2024 9:16 AM UTC

Hi @jasonj2,

 

The sound / SAI / Codec DT configuration looks good.

Could you please cross-check the SAI2_MCLK PIN configuration (should be in sai2a_pins_mx) is aligned with your hardware ?

 

Do you have an idea about why it takes so much time for the codec to be probed ? I noticed a lot of PROBE_DEFER which means that the driver is waiting something.....

 

Regarding the MCLK error : I would check with a scope if the the MCLK is really there or not : it would help to understand if the problem comes from SAI (clock, pin muxing configuration), or from the codec.

 

BTW, did you check if function wm8988_set_dai_sysclk() was called during codec driver init ?

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

3 replies

Christophe Guibout
ST Technical Moderator
Jun 6, 2024 9:16 AM UTC

Hi @jasonj2,

 

The sound / SAI / Codec DT configuration looks good.

Could you please cross-check the SAI2_MCLK PIN configuration (should be in sai2a_pins_mx) is aligned with your hardware ?

 

Do you have an idea about why it takes so much time for the codec to be probed ? I noticed a lot of PROBE_DEFER which means that the driver is waiting something.....

 

Regarding the MCLK error : I would check with a scope if the the MCLK is really there or not : it would help to understand if the problem comes from SAI (clock, pin muxing configuration), or from the codec.

 

BTW, did you check if function wm8988_set_dai_sysclk() was called during codec driver init ?

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
jasonj2
jasonj2Author
Associate III
Jun 28, 2024 4:46 PM UTC

Hi@Christophe Guibout 

(1) I checked the PIN configuration, I think it is right. Here is the PIN configuration for sai2a/b

 sai2a_pins_mx: sai2a_mx-0 {
 pins {
 pinmux = <STM32_PINMUX('I', 4, AF10)>, /* SAI2_MCLK_A */
 <STM32_PINMUX('I', 5, AF10)>, /* SAI2_SCK_A */
 <STM32_PINMUX('I', 6, AF10)>, /* SAI2_SD_A */
 <STM32_PINMUX('I', 7, AF10)>; /* SAI2_FS_A */
 bias-disable;
 drive-push-pull;
 slew-rate = <0>;
 };
 };

 sai2a_sleep_pins_mx: sai2a_sleep_mx-0 {
 pins {
 pinmux = <STM32_PINMUX('I', 4, ANALOG)>, /* SAI2_MCLK_A */
 <STM32_PINMUX('I', 5, ANALOG)>, /* SAI2_SCK_A */
 <STM32_PINMUX('I', 6, ANALOG)>, /* SAI2_SD_A */
 <STM32_PINMUX('I', 7, ANALOG)>; /* SAI2_FS_A */
 };
 };

 sai2b_pins_mx: sai2b_mx-0 {
 pins {
 pinmux = <STM32_PINMUX('G', 10, AF10)>; /* SAI2_SD_B */
 bias-disable;
 drive-push-pull;
 slew-rate = <0>;
 };
 };

 sai2b_sleep_pins_mx: sai2b_sleep_mx-0 {
 pins {
 pinmux = <STM32_PINMUX('G', 10, ANALOG)>; /* SAI2_SD_B */
 };
 };

 

(2) Yes, there is some PROBE_DEFER. I checked it, they are produced by wm8988_i2c_probe() because it cannot get MCLK from SAI (), but it looks it can finally get MCLK after tries. I don't know why.

	wm8988->mclk_handle = devm_clk_get(&i2c->dev, "MCLK");
	if (IS_ERR(wm8988->mclk_handle)) {
		dev_err(&i2c->dev, "Failed to get MCLK from %s\n", dev_name(&i2c->dev));
		if (PTR_ERR(wm8988->mclk_handle) != -ENOENT)
			return PTR_ERR(wm8988->mclk_handle);
		wm8988->mclk_handle = NULL;
	}

 

(3) I confirm wm8988_set_dai_sysclk() was called with freq=0, because there are log looks like "wm8988 1-001b: could not set sysclk, freq = 0" which is a debug output I made in the source code.

 

Sorry, I clicked the "Accept as Solution" by mistake. The problem still remains.

 

 

Best regards,

JasonJ

Christophe Guibout
ST Technical Moderator
Jul 1, 2024 2:57 PM UTC

Hello @jasonj2,

 

I will try to summarize : 

- The SAI configuration looks good

- The Codec configuration looks good

- Several probe_defer because SAI doesn't seem to provide MCLK, but after a while, it seems to be there.

 

For me, we need to know if the MCLK signal is really there on the wire:

- if yes, we need to focus on the codec

- if no, we need to focus on SAI

- if no, and after a while yes, understand what is the event which enables the clock so late.

 

BR

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.