Skip to main content
Associate II
Sep 22, 2024 3:56 PM UTC
Question

Regarding J1939 Support for STM32MP157D-DK1 Board

Hello,

 

I am trying to see if I can enable the J1939 protocols on the stm32 mp158d-dk1 board. I used the menuconfig to update the setting.

 

meme002_1-1726981454283.png

After doing that I updated the uimage, dtb, and modules to the stm32 mp1 device.

 

 

root@stm32mp1:/# dmesg | grep -i can
[ 0.256925] CAN device driver interface
[ 0.322146] can: controller area network core
[ 0.322257] NET: Registered PF_CAN protocol family
[ 0.322272] can: raw protocol
[ 0.322285] can: broadcast manager protocol
[ 0.322300] can: netlink gateway - max_hops=1
[ 0.322537] can: SAE J1939
[ 2.012003] m_can_platform 4400e000.can: m_can device registered (irq=50, version=32)
[ 2.411352] remoteproc remoteproc0: cannot get detach mbox
[ 369.920763] IPv6: ADDRCONF(NETDEV_CHANGE): can0: link becomes ready

 

 


I can see that SAE J 1939 protocol is active. I used the following headers to read from the linux user land.

 

 

 

#include<linux/can/j1939.h> // I got no errors with the header file.
#include <sys/ioctl.h>
#include <sys/socket.h>
#include <linux/can.h>
#include <linux/can/j1939.h>

#define MAX_CAN_DLC 8

int main() {
 int sock;
 int ret;
 struct sockaddr_can sockname;
 struct sockaddr_can peername;
 socklen_t peernamelen;
 struct ifreq ifr;
 uint8_t dat[128]; // Buffer to hold the received data
 int value = 1; // Enable promiscuous mode

 // Open a socket for J1939 protocol
 sock = socket(AF_CAN, SOCK_DGRAM, CAN_J1939);
 if (sock < 0) {
 perror("Socket creation failed");
 return 1;
 }

 // Specify the CAN interface (e.g., "can0")
 strcpy(ifr.ifr_name, "can0");
 ret = ioctl(sock, SIOCGIFINDEX, &ifr);
 if (ret < 0) {
 perror("ioctl failed");
 close(sock);
 return 1;
 }
 printf("CAN interface index: %d\n", ifr.ifr_ifindex);

 

 

I was wondering if anyone has success with j1939 protocol. I tried doing it, but I don't see any decoded frames in the user land.

 

Did anyone have success with J1939? If not I am planning to just use the regular CAN for my application.

Thanks

 

This topic has been closed for replies.