Skip to main content
Associate
Oct 16, 2026 7:33 AM UTC
Question

Reading EEPROM Data in U-Boot SPL

Hai,

 

I am trying to read the data stored in the EEPROM via I²C during the U-Boot SPL stage.

The EEPROM data can be read successfully from both U-Boot and user space, as shown below.

 

Uboot Area:

iWave-G62H>
iWave-G62H> i2c dev 0
Setting bus to 0
iWave-G62H> i2c md 0x50 0x0000.2 1
0000: 99    .
iWave-G62H> i2c md 0x50 0x0000.2 1
0000: 99    .
iWave-G62H> i2c mw 0x50 0x0000.2 0x01 1
iWave-G62H>
iWave-G62H> i2c md 0x50 0x0000.2 1     
0000: 01    .
iWave-G62H> i2c md 0x50 0x0000.2 1
0000: 01    .
iWave-G62H>

 

User Space:

root@imx91-iwg62h:~#
root@imx91-iwg62h:~# dd if=/sys/bus/i2c/devices/0-0050/eeprom bs=1 count=1 2>/dev/null | hexdump -C
00000000  01                                                |.|
00000001
root@imx91-iwg62h:~#
root@imx91-iwg62h:~#
root@imx91-iwg62h:~# printf '\x99' | dd of=/sys/bus/i2c/devices/0-0050/eeprom bs=1 count=1                                                                                                                         
1+0 records in
1+0 records out
1 byte copied, 0.00047425 s, 2.1 kB/s
root@imx91-iwg62h:~#
root@imx91-iwg62h:~#
root@imx91-iwg62h:~# dd if=/sys/bus/i2c/devices/0-0050/eeprom bs=1 count=1 2>/dev/null | hexdump -C
00000000  99                                                |.|
00000001
root@imx91-iwg62h:~#

 

However, the issue is that the SPL implementation is not retrieving the correct EEPROM value. Regardless of how many times I attempt to read the data using the implementation below, it consistently returns 0x00 instead of the expected value.

 

The SPL logs are provided below for reference.
U-Boot SPL 2025.04-g83e346594a6d-dirty (Oct 16 2026 - 07:26:28 +0000)
SPL: EEPROM value = 0x00
SPL: Read value: 0x00

 

Could you please review the implementation in the U-Boot SPL code and confirm whether it is correct? Additionally, could you suggest how to retrieve the expected EEPROM value during the SPL stage?

 

I have also attached the implementation added to the SPL section of the U-Boot source code.

static int read_eeprom_value(u8 *value)
{
struct udevice *chip;
int ret;

ret = i2c_get_chip_for_busnum(0, 0x50, 2, &chip);
if (ret)
{
printf("SPL: Failed to access EEPROM: %d\n", ret);
return ret;
}

/* Read 1 byte from EEPROM offset 0x0000 */
ret = dm_i2c_read(chip, 0x0000, value, 1);
if (ret)
{
printf("SPL: EEPROM read failed: %d\n", ret);
return ret;
}

printf("SPL: EEPROM value = 0x%02X\n", *value);

return 0;
}


void board_init_f(ulong dummy)
{
int ret;

/* Clear the BSS. */
memset(__bss_start, 0, __bss_end - __bss_start);

timer_init();
arch_cpu_init();
board_early_init_f();
spl_early_init();
preloader_console_init();


u8 eeprom_value = 0xFF;
ret = read_eeprom_value(&eeprom_value);

if (ret == 0)
{
printf("SPL: Read value: 0x%02X\n", eeprom_value);
}
else
{
printf("SPL: Failed to read EEPROM value\n");
}

}

 

Thank you

6 replies

Explorer
Oct 17, 2026 8:50 AM UTC

Hi ​@RobinMS ,

 

Is at least I²C support enabled in SPL (CONFIG_SPL_I2C=y) in the board configuration? 

RobinMSAuthor
Associate
Oct 17, 2026 8:58 AM UTC

Hi ​@JohannesK ,

 

I²C is enabled in the board configuration with CONFIG_SPL_I2C=y.

Are there any additional configurations that need to be enabled to read EEPROM data successfully in SPL?

Explorer
Oct 17, 2026 9:27 AM UTC

Hi ​@RobinMS !

 

Because you use the dm_i2c_*() functions it could be possible that you also must enable the U-Boot device subsystem (CONFIG_SPL_DM and also CONFIG_SPL_DM_I2C) in SPL.

But it’s only a guess. But I don’t know if you also must call the U-Boot DM initialization routines in your board init function to get the device subsystem to work.

Good luck!

 

 

RobinMSAuthor
Associate
Oct 19, 2026 11:42 AM UTC

 

Dear ​@JohannesK 

 

Please find the below details regarding EEPROM

EEPROM : M24C32

I²C bus :  0

Slave address :  0x50