Skip to main content
asadullah4571
Associate III
Oct 14, 2024 9:52 AM UTC
Question

qt-wpe-simple-browser error with wpewebkit-qtwpe-qml-plugin

Hi
i try to install qt-wpe-simple-browser on my board but it fails with error  wpewebkit-qtwpe-qml-plugin.

 

ERROR: st-image-qt-1.0-r0 do_rootfs: Unable to install packages. Command '/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-qt/1.0-r0/recipe-sysroot-native/usr/bin/apt-get install --allow-downgrades --allow-remove-essential --allow-change-held-packages --allow-unauthenticated --no-remove apt cog dpkg packagegroup-base-extended packagegroup-core-boot packagegroup-core-eclipse-debug packagegroup-core-ssh-dropbear packagegroup-core-tools-profile packagegroup-framework-core packagegroup-framework-core-base packagegroup-framework-core-extra packagegroup-framework-tools packagegroup-framework-tools-base packagegroup-optee-core packagegroup-optee-test packagegroup-st-demo packagegroup-x-linux-qt psplash-drm qt-wpe-simple-browser qtbase-plugins qtwayland-plugins resize-helper run-postinsts wpewebkit wpewebkit-qtwpe-qml-plugin' returned 100:
Reading package lists...
Building dependency tree...
Reading state information...
Package wpewebkit-qtwpe-qml-plugin is not available, but is referred to by another package.
This may mean that the package is missing, has been obsoleted, or
is only available from another source

E: Package 'wpewebkit-qtwpe-qml-plugin' has no installation candidate

ERROR: Logfile of failure stored in: /home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-qt/1.0-r0/temp/log.do_rootfs.18362
ERROR: Task (/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/layers/meta-st/meta-st-x-linux-qt/recipes-st/images/st-image-qt.bb:do_rootfs) failed with exit code '1'
NOTE: Tasks Summary: Attempted 8801 tasks of which 8774 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds

Summary: 1 task failed:
/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/layers/meta-st/meta-st-x-linux-qt/recipes-st/images/st-image-qt.bb:do_rootfs
Summary: There were 3 WARNING messages.
Summary: There was 1 ERROR message, returning a non-zero exit code.


 

This topic has been closed for replies.

2 replies

PPAGE.13
ST Employee
Oct 18, 2024 2:22 PM UTC

Qt-wpe is no more supported.

You can try a PyQt5 based browser.

If you plan to browse only in a kiosk mode, you can try the Qt official example:
https://doc.qt.io/qt-5/qtwebengine-webengine-quicknanobrowser-example.html

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
asadullah4571
Associate III
Oct 19, 2024 11:32 AM UTC

Hi @PPAGE.13 
Thanks for your respone,

Actually i can not use the https://doc.qt.io/qt-5/qtwebengine-webengine-quicknanobrowser-example.html

this one , because of the Qtwebengine , in yocto layers , meta- python2 , no more support or branch in mickledore,

So i moved on yocto 23.06.21(v5.0.1) , where i download the starter package and i installed the python3-pyqt5, 
where i successfully displayed the web-browser , but it issueing with the browser playing video , also i try to play the video using the GST play , but fails,

so as of now i am using the yocto 23.06.21 version , and debugging the GStreamer1.0, i am using the distribution package.

No more support on latest version , there is many error and bugs, with wpewebkit , qtwebengine,qt-wpe, and many more ,