Skip to main content
Associate II
Jun 6, 2025 12:55 PM UTC
Question

PyQt5 on OpenSTLinux 6.6 (Yocto Scarthgap v24.11.06) – LONG_BIT Error During Compile

Platform:

Yocto version: openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06

Machine: stm32mp1

Build environment: Ubuntu 22.04

Target image: st-image-weston

 

Summary:
I'm attempting to integrate PyQt5 into the latest ST OpenSTLinux (Scarthgap-based) BSP. While the build proceeds fine up to qtbase, the compilation fails when reaching python3-pyqt5, due to a LONG_BIT platform-related error.

 

Steps Followed:

1. repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06
2. repo sync
3. git clone https://github.com/meta-qt5/meta-qt5.git -b scarthgap ( copied into layers folder)
4.DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
5. bitbake-layers add-layer layers/meta-openembedded/meta-python
6. bitbake-layers add-layer layers/meta-qt5
7. Added IMAGE_INSTALL:append = " python3-pyqt5" in  conf/local.conf

8. bitbake st-image-weston

 

local.conf Additions:

# GPU / Qt5 related config
DISTRO_FEATURES:append = " opengl"
PACKAGECONFIG:append:pn-qtbase = " gles2 eglfs kms gbm wayland"

PACKAGECONFIG:pn-qtbase = "dbus udev evdev widgets tools libs \
freetype fontconfig gles2 eglfs kms gbm \
linuxfb accessibility sql-sqlite openssl"

# Attempt to suppress deprecated warnings
CXXFLAGS:append:pn-python3-pyqt5 = " -Wno-error=deprecated-declarations"
TARGET_CXXFLAGS:append:pn-python3-pyqt5 = " -Wno-error=deprecated-declarations"

 

PyQt5 Build Error:

After successful build of qtbase, the following occurs during bitbake st-image-weston:

#error "LONG_BIT definition appears wrong for platform (bad gcc/glibc config?)."
| 586 | #error "LONG_BIT definition appears wrong for platform (bad gcc/glibc config?)."
The failing task:
ERROR: Task (/layers/meta-qt5/recipes-python/pyqt5/python3-pyqt5_5.15.10.bb:do_compile) failed with exit code '1'

 

Request for Guidance:
Is this issue related to architecture mismatch, gcc-glibc config, or a PyQt5/meta-qt5 compatibility issue?

Has anyone successfully built PyQt5 on ST's Scarthgap (6.6) Yocto release?

Are there any recommended patches or workarounds for LONG_BIT issues in PyQt5 for STM32MP1?

Any help or direction would be greatly appreciated.

 

Thanks,

Sumithra.S

 

This topic has been closed for replies.

1 reply

PPAGE.13
ST Employee
Jun 18, 2025 10:17 AM UTC

Hi,

 

As Qt5 support is going to end soon, I would recommend to go to "python3-pyside6" with Qt6.

https://layers.openembedded.org/layerindex/recipe/380679

 

Our X-LINUX-Qt package now supports Qt6 (6.6.3) for both MP1 and MP2 families.

Updated documentation has just been released:

https://wiki.st.com/stm32mpu/wiki/X-LINUX-QT_Expansion_Package

 

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.