Skip to main content
asadullah4571
Associate III
Oct 14, 2024 9:07 AM UTC
Question

pyqt5 compile error on stm32mp1

Hi 
i tried to compile python3-pyqt5 , in my stm32mp157f-dk2 board but failed to compile. 
in my local.conf file i added this line but again fail.

IMAGE_INSTALL:append = " python3-pyqt5"
Note:  i want any browser just i want to check that URL is working or not with GUI .
please check the logs and please let me know where i am missing. 

bitbake st-image-qt
NOTE: Started PRServer with DBfile: /home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/cache/prserv.sqlite3, Address: 127.0.0.1:41977, PID: 4196
Loading cache: 100% |###########################################################################################################| Time: 0:00:00
Loaded 4738 entries from dependency cache.
Parsing recipes: 100% |#########################################################################################################| Time: 0:00:02
Parsing of 2990 .bb files complete (2987 cached, 3 parsed). 4741 targets, 536 skipped, 0 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "2.4.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-ostl-linux-gnueabi"
MACHINE = "stm32mp1"
DISTRO = "openstlinux-weston"
DISTRO_VERSION = "4.2.4-snapshot-20241014"
TUNE_FEATURES = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"
TARGET_FPU = "hard"
DISTRO_CODENAME = "mickledore"
ACCEPT_EULA_stm32mp1 = "1"
GCCVERSION = "12.%"
PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"
meta-python
meta-oe
meta-st-x-linux-qt = "main:f4c4d38033715ee54e8051969b5394cf1f3fcfae"
meta-qt5 = "scarthgap:eb828418264a49b8d00035cb3d7b12fcea3be801"
meta-gnome
meta-multimedia
meta-networking
meta-webserver
meta-st-stm32mp
meta-st-openstlinux
meta = "main:f4c4d38033715ee54e8051969b5394cf1f3fcfae"
workspace = "main:e177135751c84af691325ba02ae3005485e4345f"

WARNING: /home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_6.1.bb:do_compile is tainted from a forced run
WARNING: /home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.8.bb:do_deploy is tainted from a forced run
WARNING: /home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/layers/meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp_2022.10.bb:do_deploy is tainted from a forced run
Initialising tasks: 100% |######################################################################################################| Time: 0:00:04
Sstate summary: Wanted 438 Local 1 Mirrors 0 Missed 437 Current 3066 (0% match, 87% complete)
NOTE: Executing Tasks

ERROR: python3-pyqt-builder-native-1.16.0-r0 do_compile: ExecutionError('/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/temp/run.do_compile.5065', 1, None, None)
ERROR: Logfile of failure stored in: /home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/temp/log.do_compile.5065
Log data follows:
| DEBUG: Executing shell function do_compile
| * Getting build dependencies for wheel...
| Traceback (most recent call last):
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/pyproject_hooks/_in_process/_in_process.py", line 353, in <module>
| main()
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/pyproject_hooks/_in_process/_in_process.py", line 335, in main
| json_out['return_val'] = hook(**hook_input['kwargs'])
| ^^^^^^^^^^^^^^^^^^^^^^^^^^^^
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/pyproject_hooks/_in_process/_in_process.py", line 118, in get_requires_for_build_wheel
| return hook(config_settings)
| ^^^^^^^^^^^^^^^^^^^^^
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/setuptools/build_meta.py", line 338, in get_requires_for_build_wheel
| return self._get_build_requires(config_settings, requirements=['wheel'])
| ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/setuptools/build_meta.py", line 320, in _get_build_requires
| self.run_setup()
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/setuptools/build_meta.py", line 335, in run_setup
| exec(code, locals())
| File "<string>", line 1, in <module>
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/setuptools/__init__.py", line 108, in setup
| return distutils.core.setup(**attrs)
| ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/setuptools/_distutils/core.py", line 147, in setup
| _setup_distribution = dist = klass(attrs)
| ^^^^^^^^^^^^
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/setuptools/dist.py", line 488, in __init__
| _Distribution.__init__(
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/setuptools/_distutils/dist.py", line 283, in __init__
| self.finalize_options()
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/setuptools/dist.py", line 912, in finalize_options
| ep(self)
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/setuptools_scm/integration.py", line 123, in infer_version
| config = Configuration.from_file(dist_name=dist_name)
| ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
| File "/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/x86_64-linux/python3-pyqt-builder-native/1.16.0-r0/recipe-sysroot-native/usr/lib/python3.11/site-packages/setuptools_scm/config.py", line 216, in from_file
| return cls(relative_to=name, **args)
| ^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
| TypeError: Configuration.__init__() got an unexpected keyword argument 'version_file'
|
| ERROR Backend subprocess exited when trying to invoke get_requires_for_build_wheel
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/layers/meta-qt5/recipes-python/pyqt5/python3-pyqt-builder-native_1.16.0.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 8523 tasks of which 8513 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds

Summary: 1 task failed:
/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/layers/meta-qt5/recipes-python/pyqt5/python3-pyqt-builder-native_1.16.0.bb:do_compile
Summary: There were 3 WARNING messages.
Summary: There was 1 ERROR message, returning a non-zero exit code.
md@pc:~/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1$

 

This topic has been closed for replies.

2 replies

PPAGE.13
ST Employee
Nov 8, 2024 2:32 PM UTC
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
asadullah4571
Associate III
Nov 11, 2024 5:18 AM UTC

Hi @PPAGE.13 

Thanks for your reply,

Actually i followed the steps as you suggested, Compilation successful but when i  launch the application browser  white page open and error come " qtnetwork error 99". 
then i open the terminal, and did this command 
board> ping www.google.com
it network is working fine, but the in qt browser it shows "qtnetwork error 99".

Thanks