Skip to main content
Srini
Associate
Nov 25, 2022 10:22 AM UTC
Question

PWM - output during Suspend mode

Hi

We are using SEEED studio 102110318 module which uses STM32MP157CAC3 processor. We want to know if there is any way we can keep processor pin PD13 pin to low state in suspend state. We want the pin to maintain low state while in sleep mode. We have added pullup on this pin in Hardware which is affecting one of our peripheral operation in sleep mode. For this reason we want this pin to be set low which will solve the issue. We do not have any other option to remove pullup in hardware as our device production is completed

PD13 is used as PWM to control LCD backlight, Is there any possibility to maintain PD13 as its runtime state during suspend mode, basically i dont want to control this pin during suspend mode

I tried in sysfs, to control autosuspend_delay_ms but im getting IO error please find below image

is there any way to control it from suspend mode?

Is there any other drivers that will support this feature?

Regards

Srini

This topic has been closed for replies.

4 replies

Jean-Marc S
ST Employee
Nov 25, 2022 11:40 AM UTC

As a complement to the post:

https://community.st.com/s/question/0D53W00001xR9YeSAK/stm32mp157cac3-setting-pd13-pin-to-low-in-sleep-mode

In openStLinux the PWR mode is selected based on the active wakeup source.

So when activating under Linux the 'suspend' state, the actual HW power mode in the chip will depend on which wakeup source is active.

In your case, I understand that the HW mode is 'standby'. hence the PD13 pin is in high impedance mode

In order to have this GPIO in another state you could change this by setting your product in LPLV-Stop mode (at the expense of consumption since VDDCORE would not be Off but at a reduced voltage level only). Your design (SEEED Studio) is using STPMIC that is able to deliver reduced VDDCORE voltage..

To do this you should use a wakeup source in Group2: PVD, AVD, IWDG, GPIO, LPTIM, DTS

(see AN5109: Table 12. Deepest power mode per wakeup source group and equivalence between Linux and STM32MP15x lines)

JM

Srini
SriniAuthor
Associate
Nov 25, 2022 2:46 PM UTC

Hi JM,

Thanks for your response,

In our product we are using "systemctl suspend" command to put the device in Sleep mode (deep sleep mode)

We are waking up the device by interrupts and POWER_ON_KEY in SOM's PMIC wake up

How to configure LPLV- Stop mode in Linux?

what is the impact if we are configuring LPLV stop mode instead of deep sleep mode?

Thanks

Srini

Jean-Marc S
ST Employee
Nov 25, 2022 5:25 PM UTC

Hello Srini,

You

could replace the lower power mode "Standby" by "LPLV-Stop"

This

is done in the DT of OPTEE or TFA

example

on an eval board: stm32mp15xx-edx.dtsi

indicate

that the lowest low power mode is LPLV-Stop

&pwr_regulators {

      system_suspend_supported_soc_modes = <

               STM32_PM_CSLEEP_RUN

               STM32_PM_CSTOP_ALLOW_LP_STOP

               STM32_PM_CSTOP_ALLOW_LPLV_STOP

               /*STM32_PM_CSTOP_ALLOW_STANDBY_DDR_SR*/

       >;

       system_off_soc_mode = <STM32_PM_CSTOP_ALLOW_STANDBY_DDR_OFF>;

       vdd-supply = <&vdd>;

       vdd_3v3_usbfs-supply = <&vdd_usb>;

};

warning

.. you also need to describe the power supply level for the power mode (not

always done)

&vddcore {

       lp-stop {

               regulator-on-in-suspend;

               regulator-suspend-microvolt = <1200000>;

       };

       lplv-stop {

               regulator-on-in-suspend;

               regulator-suspend-microvolt = <900000>;

       };

       standby-ddr-sr {

               regulator-off-in-suspend;

       };

       standby-ddr-off {

               regulator-off-in-suspend;

       };

};

Impact

on consumption could be important since the VDDCORE will always be ON (at

reduced voltage level 0.9V)

you

can check datasheet p143 and p144

https://www.st.com/resource/en/datasheet/stm32mp157c.pdf

LPLV-Stop

--> upto 25mA for worst case parts at 25deg

Standby

--> 4 to 130 uA on worst case part at 25deg

so depending on your power budget this proposal may not be possible ?

JM

Srini
SriniAuthor
Associate
Nov 28, 2022 2:47 PM UTC

Thanks JM