Skip to main content
thomas987
Associate II
Sep 28, 2021 7:23 AM UTC
Solved

pps-gpio failes to request GPIO

I've enabled pps-gpio and pps in the kernel config and added the following to the device tree:

/{
//...
 pps{
 compatible = "pps-gpio";
 gpios = <&gpiod 13 GPIO_PULL_UP>;
 status = "okay";
 };
};

but this results in the following when starting the system:

[ 1.350093] pps-gpio pps: failed to request PPS GPIO
[ 1.350132] pps-gpio: probe of pps failed with error -22

do you have any hint for me how i can fix that?

I also tried adding a pinctrl section (which resulted in other problems).

Thanks!

Thomas

This topic has been closed for replies.
OlivierK
OlivierKBest answer
ST Technical Moderator
Oct 5, 2021 1:25 PM UTC

Hi Thomas,

Indeed, documentation is clear on the DT syntax and is apparently not deprecated. So I used the same DT node you used with same pins (exactly as you did), updated the linux menuconfig to enable all the pps options, recompiled the kernel and tested on a STM32MP157C-DK2 board.

did an update of the modules (depmod -a, sync). Everything looks fine.

root@stm32mp1:~# dmesg | grep pps                        

[  0.145980] pps_core: LinuxPPS API ver. 1 registered             

[  0.145998] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giom>

[  12.644460] pps_core: source pps.-1 got cdev (251:0)             

[  12.644496] pps pps0: new PPS source pps.-1                  

[  12.647391] pps pps0: Registered IRQ 88 as PPS source 

root@stm32mp1:~# lsmod | grep pps                        

pps_gpio        16384 0  

root@stm32mp1:~# cat /proc/interrupts | grep pps                 

 88:     0     0 stm32gpio 13 Edge   pps.-1  

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

7 replies

OlivierK
ST Technical Moderator
Sep 29, 2021 4:21 PM UTC

Hello thomas987 (Community Member)

 PB5 ou PG8 are the pins for the pps-out signals. Why do you use PD13?

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
thomas987
thomas987Author
Associate II
Sep 30, 2021 9:25 AM UTC

Hi,

the pps-gpio module is used for pps input -- to measure and timestamp an incoming PPS signal. It actually should work with any GPIO pin but it always fails here:

https://github.com/STMicroelectronics/linux/blob/v5.10-stm32mp/drivers/pps/clients/pps-gpio.c#L110

at the devm_gpiod_get call.

Best Regards

Thomas

OlivierK
ST Technical Moderator
Sep 30, 2021 4:50 PM UTC

Hi Thomas,

ok I understand now.

data->gpio_pin = devm_gpiod_get(&pdev->dev, NULL, GPIOD_IN);

instead of "NULL" I would expect "pps" instead. (parsing the DT for pps-gpios then extract the gpio pin).

I will check this point.

Best Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
thomas987
thomas987Author
Associate II
Oct 1, 2021 9:04 AM UTC

Hi Oliver,

> instead of "NULL" I would expect "pps" instead. (parsing the DT for pps-gpios then extract the gpio pin).

the second parameter should only specify the name used for the gpio handle, right? so "pps" would look for "pps-gpios" and NULL should look for "gpios" in the device tree like I specified: `gpios = <&gpiod 13 GPIO_PULL_UP>;`.

> I will check this point.

Thanks!

Best Regards,

Thomas

OlivierK
OlivierKBest answer
ST Technical Moderator
Oct 5, 2021 1:25 PM UTC

Hi Thomas,

Indeed, documentation is clear on the DT syntax and is apparently not deprecated. So I used the same DT node you used with same pins (exactly as you did), updated the linux menuconfig to enable all the pps options, recompiled the kernel and tested on a STM32MP157C-DK2 board.

did an update of the modules (depmod -a, sync). Everything looks fine.

root@stm32mp1:~# dmesg | grep pps                        

[  0.145980] pps_core: LinuxPPS API ver. 1 registered             

[  0.145998] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giom>

[  12.644460] pps_core: source pps.-1 got cdev (251:0)             

[  12.644496] pps pps0: new PPS source pps.-1                  

[  12.647391] pps pps0: Registered IRQ 88 as PPS source 

root@stm32mp1:~# lsmod | grep pps                        

pps_gpio        16384 0  

root@stm32mp1:~# cat /proc/interrupts | grep pps                 

 88:     0     0 stm32gpio 13 Edge   pps.-1  

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
thomas987
thomas987Author
Associate II
Oct 7, 2021 8:13 AM UTC

Hi,

thanks for checking!

Yes, indeed, it seems to work now as a kernel module (=m) but fails when i build it into the kernel (=y)

Best Regards and thanks for your help!

Thomas

axel101
Associate III
Jan 26, 2022 5:17 AM UTC

I have a same problem. The reason is that GPIO controller probes later then PPS. Initialization order is correct, but platrofm_devices are probed in different order. I fixed order by adding

pinctrl-names = "default";
pinctrl-0 = <&pinctrl>;

in y pps node. Note that if you using piz, you should set &pinctrl_z instead of &pinctrl.

I'm not sure is it solution or workaround, because I seen another configuration in iMX devicetree examples:

pps {
	pinctrl-names = "default";
	pinctrl-0 = <&pps_pins>;
	gpios = <&gpioi 10 GPIO_ACTIVE_HIGH>;
	compatible = "pps-gpio";
	status = "okay";
};
 
&pinctrl {
	pps_pins: pps_pins-0 {
		pins {
			pinmux = <STM32_PINMUX('I', 10, GPIO)>;
		};
	};
};
 

But in this case devm_gpiod_get in PPS driver says that this GPIO pin already requested by PPS driver (and after reading the sysfs I was convinced that this was the case ), and I don't know how I can get the gpio descriptor already requested in the driver.