Skip to main content
AShva.1
Associate III
Apr 22, 2020 11:35 AM UTC
Question

Openbox-session not started :(

Hi!

I installed st-example-image-x11 on the board STM32MP157x-DK2.

I can not log in :(

In the comments, I read that I need to fix the rootfs / etc / lxdm / lxdm.conf file.

Here is the file with my corrections

[base]

## uncomment and set autologin username to enable autologin

autologin=root

## uncomment and set timeout to enable timeout autologin,

## the value should >=5

#timeout=10

## default session or desktop used when no systemwide config

#session=/usr/bin/startlxde

session=/usr/bin/openbox-session

## uncomment and set to set numlock on your keyboard

# numlock=0

## set this if you don't want to put xauth file at ~/.Xauthority

# xauth_path=/tmp

# not ask password for users who have empty password

skip_password=1

## greeter used to welcome the user

greeter=/usr/libexec/lxdm-greeter-gtk

[server]

## arg used to start xserver, not fully function

arg=/usr/bin/X -s 0

# uncomment this if you really want xserver listen to tcp

# tcp_listen=1

# uncoment this if you want reset the xserver after logou

# reset=1

[display]

## gtk theme used by greeter

gtk_theme=Clearlooks

## background of the greeter

# bg=/usr/share/backgrounds/default.png

## if show bottom pane

bottom_pane=1

## if show language select control

lang=1

## if show keyboard layout select control

keyboard=0

## the theme of greeter

theme=Industrial

[input]

[userlist]

## if disable the user list control at greeter

disable=0

## whitelist user

white=root

## blacklist user

black=

I think the window manager name is incorrect (highlighted in black)

I did not find a file named openbox-session in the /usr/bin/ directory.

What you need to do to log in to the system?

Best regard

Alexander

This topic has been closed for replies.

2 replies

mleo
Visitor II
Apr 28, 2020 7:45 AM UTC

Hi Alexander,

The issue was reproduces and exoerts asked for help.

I'll come back to you when reaply is available.

Milan

AShva.1
AShva.1Author
Associate III
Apr 28, 2020 8:06 AM UTC

Hi Milan!

I solved this problem. :)

The image st-example-image-x11 uses the MATCHBOX window manager.

The line should be like this:

session=/usr/bin/matchbox-session

Best regard

Alexander

P.S.

A new problem has appeared: can't change matchbox-panel orientation :(