Skip to main content
Associate II
Jan 7, 2025 10:42 AM UTC
Solved

official u-boot tag for STM32MP157F-DK2 hangs

hi all,

 

I am using

toolchain: http://sources.buildroot.net/toolchain-external-arm-arm/arm-gnu-toolchain-13.3.rel1-x86_64-arm-none-linux-gnueabihf.tar.xz

u-boot: git clone -b v2023.10-stm32mp https://github.com/STMicroelectronics/u-boot.git

TF: git clone -b v2.10-stm32mp-r1 https://github.com/STMicroelectronics/arm-trusted-firmware.git

 

export CROSS_COMPILE to extracted toolchain: arm-gnu-toolchain-13.3.rel1-x86_64-arm-none-linux-gnueabihf/bin/arm-none-linux-gnueabihf-

Build u-boot

make ARCH=arm stm32mp15_defconfig

make DEVICE_TREE=stm32mp157f-dk2

TF:

make PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 STM32MP_SDMMC=1 STM32MP_EMMC=1 AARCH32_SP=sp_min DTB_FILE_NAME=stm32mp157f-dk2.dtb BL33_CFG=../u-boot/u-boot.dtb BL33=../u-boot/u-boot-nodtb.bin all fip

 

copy the generated tf-a-stm32mp157f-dk2.stm32 and the fip.bin to the fsbl1 fsbl2 and fip partitions of the SD card.

 

On board it hangs on

NOTICE: BL2: Booting BL32

 

Do I need some additional menuconfig to set for u-boot?

Exactly same steps (except using stm32mp157c-dk2, DEVICE_TREE=stm32mp157c-dk2 and DTB_FILE_NAME=stm32mp157f-dk2.dtb ) for

git clone -b v2024.10 https://source.denx.de/u-boot/u-boot.git

git clone -b v2.12.0 https://git.trustedfirmware.org/TF-A/trusted-firmware-a.git

works perfectly.

 

regards

 

This topic has been closed for replies.
anpaBest answer
Associate II
Jan 15, 2025 7:36 PM UTC

Found the solution. Obviously AARCH32_SP=sp_min is not supported anymore so right way is:

git clone -b 4.0.0-stm32mp-r1 https://github.com/STMicroelectronics/optee_os.git
git clone -b v2023.10-stm32mp-r1 https://github.com/STMicroelectronics/u-boot.git
git clone -b v2.10-stm32mp-r1 https://github.com/STMicroelectronics/arm-trusted-firmware.git
cd optee_os
export CROSS_COMPILE=<path to toolchain>
make ARCH=arm PLATFORM=stm32mp1 CFG_EMBED_DTB_SOURCE_FILE=stm32mp157f-dk2.dts
cd ../u-boot
make ARCH=arm stm32mp15_defconfig
make DEVICE_TREE=stm32mp157f-dk2
cd ../arm-trusted-firmware/
make PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 DTB_FILE_NAME=stm32mp157f-dk2.dtb STM32MP_SDMMC=1
make PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 AARCH32_SP=optee DTB_FILE_NAME=stm32mp157f-dk2.dtb BL33=../u-boot/u-boot-nodtb.bin BL33_CFG=../u-boot/u-boot.dtb BL32=../optee_os/out/arm-plat-stm32mp1/core/tee-header_v2.bin BL32_EXTRA1=../optee_os/out/arm-plat-stm32mp1/core/tee-pager_v2.bin BL32_EXTRA2=../optee_os/out/arm-plat-stm32mp1/core/tee-pageable_v2.bin fip

 create sd card image.

3 replies

anpaAuthor
Associate II
Jan 7, 2025 10:45 AM UTC

also the official fip/fip-stm32mp157f-dk2-opteemin-sdcard.bin works perfectly when I copy to the fip partition. Maybe dump the config and compare?

anpaAuthor
Associate II
Jan 8, 2025 9:45 AM UTC

Unfortunately fip-stm32mp157f-dk2-opteemin-sdcard.bin doesnt have config command configured so can not dump the settings.

BTW there is a small error in first post:

 

"

Do I need some additional menuconfig to set for u-boot?

Exactly same steps (except using stm32mp157c-dk2, DEVICE_TREE=stm32mp157c-dk2 and DTB_FILE_NAME=stm32mp157f-dk2 stm32mp157c-dk2.dtb ) for

git clone -b v2024.10 https://source.denx.de/u-boot/u-boot.git

git clone -b v2.12.0 https://git.trustedfirmware.org/TF-A/trusted-firmware-a.git

works perfectly.

anpaAuthorBest answer
Associate II
Jan 15, 2025 7:36 PM UTC

Found the solution. Obviously AARCH32_SP=sp_min is not supported anymore so right way is:

git clone -b 4.0.0-stm32mp-r1 https://github.com/STMicroelectronics/optee_os.git
git clone -b v2023.10-stm32mp-r1 https://github.com/STMicroelectronics/u-boot.git
git clone -b v2.10-stm32mp-r1 https://github.com/STMicroelectronics/arm-trusted-firmware.git
cd optee_os
export CROSS_COMPILE=<path to toolchain>
make ARCH=arm PLATFORM=stm32mp1 CFG_EMBED_DTB_SOURCE_FILE=stm32mp157f-dk2.dts
cd ../u-boot
make ARCH=arm stm32mp15_defconfig
make DEVICE_TREE=stm32mp157f-dk2
cd ../arm-trusted-firmware/
make PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 DTB_FILE_NAME=stm32mp157f-dk2.dtb STM32MP_SDMMC=1
make PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 AARCH32_SP=optee DTB_FILE_NAME=stm32mp157f-dk2.dtb BL33=../u-boot/u-boot-nodtb.bin BL33_CFG=../u-boot/u-boot.dtb BL32=../optee_os/out/arm-plat-stm32mp1/core/tee-header_v2.bin BL32_EXTRA1=../optee_os/out/arm-plat-stm32mp1/core/tee-pager_v2.bin BL32_EXTRA2=../optee_os/out/arm-plat-stm32mp1/core/tee-pageable_v2.bin fip

 create sd card image.