Skip to main content
Senior
Oct 18, 2026 11:01 PM UTC
Question

No support for vkEnumerateInstanceVersion - vilkan falls back to 1.0?

Hi!

 

When I run the command "vulkaninfo --summary". I get this critical error.

"libvulkan_VSI.so.1.3.3 contained a 1.1 or greater API version, but does not support vkEnumerateInstanceVersion, treating as a 1.0 ICD".

What this means is that according to the data sheet of STM32MP2, the GPU supports Vulkan 1.3. but due to the lack of support for vkEnumerateInstanceVersion, the Vulkan support falls back to 1.0.

Question: is this true that Vulkan falls back to 1.0 fue to this warning?

Is there any newer version of libvulkan_VSI.so?

Here is the complete output: 

"""

WARNING: [Loader Message] Code 0 : loader_scanned_icd_add: Driver /vendor/lib/libvulkan_VSI.so.1.3.3 supports Vulkan 1.3, but only supports loader interface version 2. Interface version 5 or newer required to support this version of Vulkan (Policy #LDP_DRIVER_7)

WARNING: [Loader Message] Code 0 : terminator_CreateInstance: Manifest ICD for "/vendor/lib/libvulkan_VSI.so.1.3.3" contained a 1.1 or greater API version, but does not support vkEnumerateInstanceVersion, treating as a 1.0 ICD

WARNING: [Loader Message] Code 0 : terminator_CreateInstance: Driver /vendor/lib/libvulkan_VSI.so.1.3.3 supports interface version 2 but still exposes VkSurfaceKHR create/destroy entrypoints (Policy #LDP_DRIVER_8)

==========

VULKANINFO

==========

 

Vulkan Instance Version: 1.3.275

 

 

Instance Extensions: count = 12

-------------------------------

VK_EXT_debug_report : extension revision 10

VK_EXT_debug_utils : extension revision 2

VK_KHR_device_group_creation : extension revision 1

VK_KHR_display : extension revision 23

VK_KHR_external_fence_capabilities : extension revision 1

VK_KHR_external_memory_capabilities : extension revision 1

VK_KHR_external_semaphore_capabilities : extension revision 1

VK_KHR_get_physical_device_properties2 : extension revision 2

VK_KHR_portability_enumeration : extension revision 1

VK_KHR_surface : extension revision 25

VK_KHR_wayland_surface : extension revision 6

VK_LUNARG_direct_driver_loading : extension revision 1

 

Instance Layers:

----------------

 

Devices:

========

GPU0:

 apiVersion = 1.3.0

 driverVersion = 6.4.21

 vendorID = 0x10002

 deviceID = 0x80006205

 deviceType = PHYSICAL_DEVICE_TYPE_INTEGRATED_GPU

 deviceName = VeriSilicon 

 driverID = DRIVER_ID_MESA_RADV

 driverName = VERISILICON

 driverInfo = 6.4.21.1.1058597

 conformanceVersion = 1.3.5.0

 deviceUUID = 0062008c-7d09-47bb-b5d1-0ac5c5b13c85

 driverUUID = 06041525-7d09-47bb-b5d1-0ac5c5b13c85

""" 

2 replies

PPAGE.13
ST Employee
Nov 5, 2026 2:35 PM UTC

Hello,

There is no more up-to-date library release available. I confirm the warning.

I have submitted the question to the Verisilicon development team and will keep you informed.

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
WindowsAuthor
Senior
Nov 5, 2026 2:58 PM UTC

​@PPAGE.13 

Thank you!

Very good! I'm waiting for a reply.