Skip to main content
This topic has been closed for replies.
Bernard PUEL
Bernard PUELBest answer
ST Technical Moderator
Apr 8, 2019 1:56 PM UTC

Yocto build is not providing this file by default, so ST is not providing it in its delivery. So you will need to build the kernel to have it (but I understand this is what you don't want to do ...).

We think the safer and generic way to proceed is to make the menuconfig and rebuild the kernel with this config. This is the only way to make sure all the dependencies are well managed.

OpenSTLinux kernel is not big and you will need only 10/15 minutes to build it from scratch with the Developer package (see the link above).

3 replies

Olivier GALLIEN
ST Technical Moderator
Mar 28, 2019 3:20 PM UTC

Hi,

Did you have a look to wiki article here ?

 https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package

Section 6 Modifying/adding an external Linux kernel module might give you some clue

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MBeck
MBeckAuthor
Associate
Mar 30, 2019 9:32 PM UTC

Yes, I have seen that. This is what I am doing, but without Module.symvers you need to force insmod the resulting kernel modules. Without the file, a complete re-built of the kernel is required.

Bernard PUEL
Bernard PUELBest answer
ST Technical Moderator
Apr 8, 2019 1:56 PM UTC

Yocto build is not providing this file by default, so ST is not providing it in its delivery. So you will need to build the kernel to have it (but I understand this is what you don't want to do ...).

We think the safer and generic way to proceed is to make the menuconfig and rebuild the kernel with this config. This is the only way to make sure all the dependencies are well managed.

OpenSTLinux kernel is not big and you will need only 10/15 minutes to build it from scratch with the Developer package (see the link above).